What source file are the pins initialized?
Posted on November 10, 2017 at 21:15What source file initializes these pins?
Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Posted on November 10, 2017 at 21:15What source file initializes these pins?
Posted on November 14, 2017 at 15:11I tried to simulate the evaluation circuit of the STEVAL-ISA174V1. I have loaded the VIPER0P.LIB and have integrated it in ORCAD 17.2. During simulation I get error messages. Subcircuits DAC_2BIT, DAC_3BIT, DAC_4B...
Posted on November 12, 2017 at 10:25I've opened the P-NUCLEO-IHM001_SINGLEDRIVE project.In Control stage parameters.h I see#define PHASE_UH_GPIO_PORT GPIOA #define...
Posted on November 10, 2017 at 13:52Hello, I'm facing an issue regarding the 3.3V line on my board that embeds a stm32. The board also embeds a radio module (WISOL SFM10R1). My problem is that at one moment my radio module seems to be blown because ...
Posted on November 09, 2017 at 13:58How to bootload ♯?#stspin32f0 #stspin32f0a
Posted on November 09, 2017 at 13:50can ♯ used for brushed dc motors (ordinary dc motors)♯#stspin32f0 #stspin32f0a
Posted on November 07, 2017 at 22:32Hi there,I would like to design a led driver to supply a load of 100W and 150W using the HVLED001A but the eDesignSuite is not calculating the right transformer. According to datasheet of HVLED001A is possible to ...
Posted on October 31, 2017 at 00:52Hi,Please see schema below.With this circuit the cells in series are creating ~ 0.82V in office lighting.LDO2 output is only 0.5v. This does not seem right. :)Can anyone at ST help with correct selection of R1-6 s...
Posted on October 26, 2017 at 09:18The output Voltage expected is 6V and output is constant for 110VAC input. But the output is turning ON/OFF for 220V input. Please let me know to resolve this issue.
Posted on January 10, 2017 at 10:59Hello!Has anyone worked with the STEVAL-ISW001V1 demoboard or has designed an inverter welder based on the demoboard schematics? My design is working well in normal operation but I have some issues with the short-c...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.