2013-09-10 2:25 AM
Hi,
I want to drive peltier element to control temperature of one module. Peltier specifications are:Imax = 9A and Vmax = 3.75V.Such 4 peltiers are connected in series to control to module temperature.I am planning to use L298N for driving it. As shown if I connect L298N two pins in series then I will be able to drive current upto 4A. But, to control my module temperature, Peltier is sinking average 4A current.So, It I can't use single L298N IC as it will heat too much and also it will damage.So, I want to know whether it is possible to use two L298N ICs in parallel to give higher current.If so then please advice me for input and output pin connections.Thanks & Regards,Sachin PanchalWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.