2015-04-10 2:52 AM
Hi there,
I recently had a discussion on DT0001 motor control [DEAD LINK /public/STe2ecommunities/motordriver_ics/Lists/Motor%20Control%20Firmware%20and%20Software/Flat.aspx?RootFolder=/public/STe2ecommunities/motordriver_ics/Lists/Motor%20Control%20Firmware%20and%20Software/Speed%20Control%20according%20to%20DT0001&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000CE106710FFA6574FB92BFFEFCE2DD930&TopicsView=https://my.st.com/public/STe2ecommunities/motordriver_ics/Lists/Motor%2520Control%2520Firmware%2520and%2520Software/AllItems.aspx¤tviews=19]here. In the end, since I am using the L6235 to drive the motor I was wondering whether this IC is able to handle current coming back from the motor when braking. Thanks, Rasmus #dt0001 #l62352015-04-26 11:25 PM
Hi Rasmus,
until the motor current and the bus voltage stay within the absolute maximum ranges there are no issues. Basically I confirm all the suggestions from the post you linked. However, the integrated overcurrent protection does not operate in this case (it is not sesitive to ''reverse'' currents); so you cannot rely on it for the device protection. EnricoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.