2024-01-30 4:57 AM
Hi I cant figure out which is the correct Diode. It was mounted in a Charging (12/24V DC input) device for ADALIT Firefighter Light .
Thanks for your Help
Solved! Go to Solution.
2024-01-30 9:23 AM
It's a TWO LETTER MARKING CODE
https://github.com/cturvey/RandomNinjaChef/blob/main/stdiode.txt#L15 SMAJ30A CK
It's not terribly clear in your image, so an educated guess. You might be able to get a clearer image, angle, or another board with the same part. Get better imagery, or attach the original, not screen shot of another image on a phone..
See also "DIODES INC" brand
2024-01-30 5:39 AM - edited 2024-01-30 9:24 AM
CK ?
SMBJ30(C)A
2024-01-30 7:46 AM
what does CK mean?
2024-01-30 9:23 AM
It's a TWO LETTER MARKING CODE
https://github.com/cturvey/RandomNinjaChef/blob/main/stdiode.txt#L15 SMAJ30A CK
It's not terribly clear in your image, so an educated guess. You might be able to get a clearer image, angle, or another board with the same part. Get better imagery, or attach the original, not screen shot of another image on a phone..
See also "DIODES INC" brand
2024-01-30 9:26 AM
"G3 019"
Most likely epoxy/material related, and year/week of manufacture. The product code is the one you want to read off clearly.
2024-01-30 9:56 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.