2025-09-16 6:32 AM - last edited on 2025-09-16 7:03 AM by Andrew Neil
we want to know that. Can this IC E-Fuse capable to handle negative transients (350 ms) of -40 Volt.
Please Reply ASAP.
MPN: STEF01
Solved! Go to Solution.
2025-09-16 12:26 PM
If you are asking about a possible negative input voltage: reverse polarity protection is required for this, e.g. with a p-channel MOSFET and at -40V also a TVS or zener to limit the voltage to the maximum gate voltage. Such reverse polarity protection blocks the negative voltage and thus prevents the destruction of the downstream components, in this case the STEF01.
Regards
/Peter
2025-09-16 7:13 AM
On the output pin? The output pin is limited to -0.3 V. -40 V is far outside of these bounds. Operation outside of the absolute maximum ratings is not guaranteed.
2025-09-16 7:18 AM
@TDK wrote:Operation outside of the absolute maximum ratings is not guaranteed.
Indeed.
@PradipRaj Worse than that - operation beyond the Absolute Maxima may cause damage:
2025-09-16 7:44 AM
And in this case, will almost certainly cause damage.
The -0.3 V limit suggests protection diodes. When you try to pull a net to - 40 V, those diodes will activate and try to bring VSS to - 40 V. That in turn will almost assuredly bring other rails down.
2025-09-16 12:26 PM
If you are asking about a possible negative input voltage: reverse polarity protection is required for this, e.g. with a p-channel MOSFET and at -40V also a TVS or zener to limit the voltage to the maximum gate voltage. Such reverse polarity protection blocks the negative voltage and thus prevents the destruction of the downstream components, in this case the STEF01.
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.