Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Inquiry Regarding L9961 Datasheet

Hello, I checked the L9961 datasheet for information on the cell voltage protection function, but couldn't find the operating voltage.  Other products usually provide Over Voltage Protection (OVP) for cells, but in the case of L9961, only the cell me...

jslee by Associate II
  • 1281 Views
  • 1 replies
  • 0 kudos

Viper comp design

Hello everybody,I need to user Viper115HS or Viper222XS vith 15V 600mA output at non isolated buck topology. I was designed my Fb pin with 130K Ohm and 11K Ohm resistors. But I can not find right Comp pin configuration. could you write capasitor and ...

Mnemonic by Associate III
  • 1514 Views
  • 3 replies
  • 0 kudos

L9945TR Mosfet Pre-driver peak drive current

    Good afternoon ST engineer。I'm developing a DC motor control hardware using the L9945 in H brigde mode 。But facing a problem: the datasheet haven't any description about the Mosfet Pre-driver peak drive current when using external drive resistors...

Resolved! STPMIC1APQR does not always turn on.

I have a circuit with pmic STPMIC1APQR and STM32MP157DAA1 processor. For reference, I take STM32MP157A-EV1.There are cases when STPMIC1APQR does not turn on every time you turn on the power (1 time out of 20-50 turns on). At the same time, the input ...

vvlad.1 by Associate II
  • 4447 Views
  • 5 replies
  • 0 kudos

Nucleo L476RG External power

Hello,I have a Nucleo L476RG that I plug onto a PCB that I designed (used as a power input) and to my computer (only used for data transfert).My issue is that I would like to plug both to the Nucleo, but only use the PCB for its power supply.Moreover...

Claire2 by Associate
  • 1717 Views
  • 1 replies
  • 1 kudos

Resolved! Help identifying SMD

Hi there, I was unable to find any matching for this part below, some bi-directionnal TVS I presume, but "L06" returns nothing.I need your help ^^ thanks.Nicolas.

20240613_100218_1.jpg

Viper222 going shutdown problem

Hello everybody,I was designed a SMPS with Viper222XS for my project. I need to 400ma current for my project. its start with 100mA at soft start and going to 400mA immidiatly after pushhing run button. But I have some problem at here. SMPS was goes t...

Mnemonic_0-1718186158414.png
Mnemonic by Associate III
  • 931 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.