Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Viper115 cannot produce the required current

I am designing a new SMPS for my project I need 350mA at 15V but I could not get more than 100ma. when I reach to 100mA output voltage was start to decrease. when current goes to 200mA, output is like a sinusodial signal from 9v to 15V. I design my S...

Mnemonic_0-1717402436350.png
Mnemonic by Associate III
  • 4618 Views
  • 11 replies
  • 0 kudos

TCPP01-M12 OVP on CC lines

Good morning, I have got a couple quick questions about the TCPP01-M12 chip:Does the OVP protection on CC lines works passively? (no voltage on VCC pin) I am talking about connecting/disconnecting USB plug conditions.What happens when there is perman...

1.png 2.png
withorlo by Associate
  • 927 Views
  • 0 replies
  • 0 kudos

EVLVIPGAN100PD

I've encountered an issue while simulating a schematic in the eDsim software. I attempted to create a schematic resembling the reference design by exporting the schematic of a 100W flyback converter from the online tool of ST eDesign suite. I then ma...

nesrine12 by Associate III
  • 1185 Views
  • 0 replies
  • 0 kudos

Resolved! VNF9Q20F Grounding

From the application schematics of VNF9Q20F, seperating my ground planes for CReg and DVcc but wouldnt DEV_GND (straight from the VNF9Q20F at the bottom) be connected as well instead of to battery ground? Shown as the drawn orange connection. Or both...

DEV_GND.png
TH3221 by Associate III
  • 1958 Views
  • 3 replies
  • 1 kudos

Resolved! Power Path Selector with STMPS2141STR

Hello everyone,  I am designing a PCB and I want a power path selector which can change the source between USB and Battery.Can I do this with STMPS2141STR ? I cannot find a circuit or an application note. This is my design is that correct ? Can someb...

testbenchmark_0-1717484187060.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.