Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

EVAL-L9942 interface problem

Posted on September 18, 2014 at 17:37Hello!I bought 3 Eval-L9942 boards. I connected supply voltage (5V). Enable (connect to 5V) and a step clock (5V. 100Hz). The VS supply is 12V.The motor i have connected does not move. All outputs are at 12V cons...

stepper motor ramp profile using timer 1 output compare

Posted on August 29, 2014 at 03:19timer 1 output compare to generate Step output for stepper motorI am using timer1 channel 1 as output compare, to generate a pulse of variable period.Desire output – In the  beginning the output remain low for 4 ms(...

0690X00000603PDQAY.jpg

Implementing motion profile multiple L6470 chips

Posted on September 15, 2014 at 16:23I'm investigating using the L6470 for an multi-axis application. Please let me now if it is possible using SPI to position multiple motors according to a motion profile/position table at constant speed. i.e. impl...

thh by Associate
  • 911 Views
  • 1 replies
  • 0 kudos

Can't reliably sense stalling using L6470 chip

Posted on October 22, 2013 at 20:37I've been quite successful at controlling the L6470 stepper driver chip from my embedded ARM processor for all features other than the sensorless stall detection feature. I'm hoping that I'm missing something and t...

GoTo(ABS_POS) error during motor running

Posted on September 03, 2014 at 09:59Hello!In my application I send GoTo(ABS_POS) commands when stepper motor is running at constant speed, when BUSY flag is high, so I'm sure that the target speed is reached. And everything is going well most of ti...

srg0016 by Associate II
  • 1332 Views
  • 2 replies
  • 0 kudos

a formula about duty cycle computation

Posted on August 03, 2014 at 06:34hello all :             I,recently?found that the formula about duty cycle  computation in the SW do not accord with that in the user manual . Sector ????TimePhA=T/8+?T+X-Z?/2 in the SW,however,Sector ????TimePhA=?T...

Input Voltage limit on VNH5050 Diag/ENA pin

Posted on August 14, 2014 at 03:20HiI'm designing a very compact quad VNH5050 12V Motor Driver board.I can optimize my design if I can pull-up the DIAG/ENA pins to 12V rather than the 5V Logic level.There is nothing else connected to these pins.  Al...

Problem about L6482H (OCD failure)

Posted on August 22, 2014 at 19:45HiI have developed about motor control by using L6482H. I follow circuit form reference circuit of L6482H Eval board (same part). Now I stuck at OCD failure. I have construct a new board follow Eval board. In Eval b...

prustya by Associate
  • 593 Views
  • 0 replies
  • 0 kudos

L6207 PWM Current Control Question

Posted on July 30, 2014 at 19:04Could someone please explain how current is controlled on the L6207 via onboard PWM Current Controller?  Additionally, AN1762 APPLICATION NOTE indicated a constant current could be obtained through a simple voltage di...

dstetson by Associate
  • 904 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.