2014-07-30 10:04 AM
Could someone please explain how current is controlled on the L6207 via onboard PWM Current Controller? Additionally, AN1762 APPLICATION NOTE indicated a constant current could be obtained through a simple voltage divider into Vref.
For example, I want to cap the current at 1.5A / phase, what type of PWM or voltage division would I need to implement? Thank you. #l62072014-08-21 5:29 AM
Hello,
the current level is set according to the following formula: Iphase = Vref/Rsense where Vref is the reference voltage you set at the REF input and Rsense is the shunt resistor connected between the SENSE pin and ground. Regards EnricoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.