Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI communication problem

Posted on October 21, 2014 at 15:30hello, I have a EVAL6480H board and try to connect it with a Atmel Xmega. But on the SDO line is always the Byte which I send before on SDI. Does I Need to make some initalisation before start a communication? I c...

STEVAL-IHM032V1 and STEVAL-IHM032V1

Posted on January 22, 2016 at 08:00Hi I have the STEVAL-IHM032V1 and STEVAL-IHM039V1.The motor is T-motor U8. I have configure the U8 through ST Motor Control Workbeach. The Keil has build success.But the motor is not work. I use the Oscilloscope to...

chenwei by Associate II
  • 569 Views
  • 0 replies
  • 0 kudos

Maybe it LD1086

Posted on January 19, 2016 at 22:10Help determine the marking voltage regulator. Designation on board IC 995.

Suggestion for documentation.

Posted on January 05, 2016 at 12:21The documentation for the IHM001 should more clearly state that the included nucleoF302R8 is NOT the standard  nucleo with that processor!Because I didn't want to ''break'' the included nucleo and demo app (I could...

3 shunt current measurement

Posted on November 16, 2015 at 16:16Hi everyone,I'm using the following evaluation boards:    - STM32303C-EVAL    - STEVAL-IHM023V3I'm trying to make FOC algorithm for ACIM. The whole FW is written by myself excluding the standard peripheral lib fro...

eval-L6470 firmware

Posted on November 12, 2015 at 10:50hi, i want to know where can i get the source code for eval-L6470 board default firmware? i got fwpspin_discoveryboard_v205.hex file, it work but shows error light i want to trace the error so i need the source co...

the LCD of STEVAL-IHM022V1 disable? how to recovery?

Posted on November 18, 2015 at 16:50Recently I did LCD User Interface download according the user manual.I download the  Project\EWARM_Out\*.out binary file to my demo board STEVAL-IHM022V1, so LCD all disable. How could I recovery the LCD that disp...

Connect a PowerSTEP01 to a STM32469I-Discovery

Posted on December 08, 2015 at 21:19Hello all! I am working on using a PowerSTEP01 with a STM32469I-Discovery.  I have example code that uses a STM32F401RE-Nucleo and a X-Cube-IMH03A1 and that works great.  The thing I am working on now is the Syste...

why get differemt value of FOC's current iab?

Posted on December 18, 2015 at 04:28I used stm32 library ADC & DMA to get the FOC Ia,b values, but the values are  different at using PMSM libraryPWMC_GetPhaseCurrents(oCurrSensor[MC_NUM], &Iab); I didn't know why have different values.The values of...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.