Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BLDC commutation with hall sensors

Posted on May 30, 2014 at 17:09The original post was too long to process during our migration. Please click on the attachment to read the original post.

ssatjas9 by Associate
  • 1724 Views
  • 1 replies
  • 0 kudos

L6470H does't switch between SYNC and BUSY mode

Posted on March 12, 2016 at 19:10 Hello. I use L6470H chip. I found a issue of the chip. I want switch mode BUSY and SYNC in my program to control of the step clocking. I can write ''1'' to SYNC_EN bit of the STEP_MODE register. BUT I ca...

15V Regulator L78L15 Not Regulating

Posted on March 12, 2016 at 01:06I have some L78L15ACZ's that do not seem to be working, or perhaps there is some required external component/circuit configuration that is missing?  The output is remaining approx. a diode drop below the input...beyo...

candace by Associate
  • 527 Views
  • 0 replies
  • 0 kudos

L78M24CDT

Posted on March 10, 2016 at 17:41ST L78M24 DPAK (PFA Datasheet) has input voltage max of 40V, we are operating the part at about 39V which is very close this upper limit. Our average circuit current consumption can go upto 66mA. Actual Power Dissipa...

IGBT Short circuit withstand time

Posted on March 10, 2016 at 11:39Hello,I'm using 6 IGBT's part no. STGF10NC60KD in a typical three-phase inverter application and I have designed a short circuit protection to prevent IGBT damage when 2 phases of the motor becomes accidentally short...

HB driving for low frequency or DC (L6743)

Posted on March 08, 2016 at 11:29We have to prepare an H-Bridge to supply a resistive load in both current directionsWe plan to use 4 N-channel MOSFETs and we would like to use L6743 as a HB driver for each couple of MOSFETS But we want to use in al...

SPV1050 LDOs connected to store or to battery?

Posted on March 06, 2016 at 10:45(Text was missing in my 1st post. Did not work from mobile?)Hi - does someone know whether the two LDOs on the SPV1050 will supply power even when the charging circuitry is disconnected from the battery (!BATT_CONN i...

soren by Associate II
  • 798 Views
  • 0 replies
  • 2 kudos

L6470 OUTPUTS PROTECTION

Posted on February 18, 2016 at 11:40We have an issue related your stepper motor controller L6470.We are working with two of your evaluation boards: EVAL6470H-DISC and EVAL6470PD and we had two critical situations with two boards, one of each. In tho...

lpinion by Associate
  • 738 Views
  • 0 replies
  • 0 kudos

L6470 protection

Posted on February 11, 2016 at 13:22Hi,I have a question regarding L6470 protection. Are any protection diodes needed on the L6470 outputs?The datasheet doesn't mention any protection and the evaluation boards doesn't have any. This is the case also...

fedeja by Associate
  • 691 Views
  • 1 replies
  • 0 kudos

Questions on STEVAL-IHM038V1

Posted on January 25, 2016 at 10:29Questions on STEVAL-IHM038V1 We are planning to design a BLDC ceiling fan controller board based on the STEVAL-IHM038V1 evaluation board. (http://www.st.com/web/en/catalog/tools/PF255633) We have some technical q...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.