cancel
Showing results for 
Search instead for 
Did you mean: 

What kind of impact can demage the L6470pd in that way?

dbecher
Associate
Posted on June 27, 2016 at 13:35

Hi at all,

is there someone with an idea what has happened there with the L6470. I´ve attached 2 photos of the demaged device and on picture of the scematic sheet. It looks like the motor bridges are directly shorted to GND. The connected stepper motor is working well with an impedance of about 2.4Ω of each coil. 

The supply voltage of VSAx and VSBx is 35.5V.

Thanks for your help!

   

    
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.