Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

error while using powerSTEP01,

Posted on March 14, 2017 at 17:05 when the stepper motor got horizontal forces the powerstep01shutdown and all the status register bits turns to zeros.We work in current mode, the thresholds levels adjusted to maximum.

Vsense_nom of VNH7070AS

Posted on March 15, 2017 at 08:171�what is Vsense_nom ? How level? I find nothing in datasheet.

pan feng by Associate
  • 1143 Views
  • 2 replies
  • 0 kudos

capacitor power supply voltage drop

Posted on March 09, 2017 at 15:28Hi, i designed transformerless capacitive power supply for compact home automation project. Initially its used for only controlling load so it worked good at 4.8Vdc. Later i added seven segment display and tactile sw...

L6480 Stepper Motor Power Supplies Question

Posted on February 21, 2017 at 07:11Hello,I am looking at using the L6480 in the externally supplied modes, where my system will be supplying: VS = +24V DCVSREG/VCC = +12VVCCREG/VREG = +3.3VThe +24V supplied to VS by the system is removed (floating)...

help with the L6668

Posted on February 28, 2017 at 15:54i am looking at using the L6668 as a multy output flyback, i need it to have a high voltage start up (which this IC does have, that is good), but i also need it to synchronise it to about 100KHz from a micro.my qu...

Can the L6615 load share controller be used for 50V bus high side application? A resistor divider to reduce common mode can be used on the sense pins but how do you calculate the component values?

Posted on February 18, 2017 at 17:51I am using the L6615 in a 50V bus current sharing application and I have the required voltage divider from each side of the high side current sense resistor to ground but I am unsure if another series resistor nee...

Doubt on STM6600 use

Posted on February 13, 2017 at 20:46I want to use the STM6600 controller to manage the power ON/OFF of my microcontroller system. In the specific I want:- Turn ON the system simply pushing a button.- Turn OFF the system simply pushing the same butto...

L6472, problem with absolute position register

Posted on February 10, 2017 at 15:10HiI'm using the L6472 Eval board, revision 1.1.We got two L6472 Eval board connected to our main stm32f2 board. Both drivers are running smoothly and everything is working, but reading the absolute position regist...

L6230Q VFQFPN32 High Side Voltage Drop = 2.6V

Posted on February 08, 2017 at 15:03Hello,i our Motor Control Board with FOC i have very high losses in the Driver IC L6230Q in the VFQFPN package.In the On-Time of the High side i have a differenz of 2.6V between the Operatine Voltage (21V) and the...

s61331 by Associate II
  • 1972 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.