Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

C-Lib or include-File for L99PM72GXP ?

Posted on April 12, 2018 at 11:12hello,      I'm looking for a Library or include-File, written in C, but nothing found.    I met a problem?The main chip is reset after the watchdog resets it.    How to reset the watchdog after the main chip reset? ...

USB-C PD Library for P-NUCLEO-USB002

Posted on April 05, 2018 at 16:11Hi, I am developing a USB-C Power Delivery Consumer with VDM Support, but don't know how to use the Library for own Application. Does anyone has a manual how to use the functions from this Library?

STC3115 configuration

Posted on March 16, 2018 at 11:53Dear,Is it possible to adapt the table of SOC values in the STC3115 so I can use a 4.35V (-IQT) version in a situation where I need a 4.2V (AIQT) version of the chip? See AN4324 page 9.Regards,Roland#stc3115 #soc

STEVAL-IPE016V1 voltage measurement problem

Posted on April 10, 2018 at 15:56I'm trying to use the STEVAL-IPE016V1 to get a basic knowledge of the STPM10 chip that i would like to use for an energy meter design. Unfortunately the board was shipped with a faulty connection on the R7 resistor(t...

Low Speed Bldc 6STep Library

Posted on March 08, 2018 at 10:10HiI am using IHM08M1 board with stm32f302, to drive a bldc 36 volts BLDC motor. I am using SixSTep library (SPN8). I need very low speed in my project like 1 rpm. The motor has a 100:1 reduction gear. The minimum spe...

Can I have a PWM 5V logic signal coming into L9907?

Posted on April 03, 2018 at 04:41The L9907 datasheet states that I/O is 3.3V logic compatible.  It also states that I/O pins can withstand voltages up to 35V in the 'Absolute Maximum Ratings' section on page 17.  I was wondering if it were wise to h...

Tom B by Associate
  • 1284 Views
  • 2 replies
  • 0 kudos

Request about original marking code

Posted on April 05, 2018 at 10:26Hi,I need to know if my component is an original ST component.This is the code on my case component: B55NF06CC039     W MAR    512 I have only a photo of this component. ThanksAndrea

Controlling a sensorless 15W BLDC motor using STEVAL-SPIN3202

Posted on January 18, 2018 at 23:26I'm using a STEVAL-SPIN3202 to control a 15W BLDC sensorless motor. I'm unable to spin a motor using six-step driving mode and I'm assuming it's because the motor's configuration needs to be updated. Looking at the...

L6472 - Fixed Point Registers

Posted on June 22, 2016 at 00:19I am trying to find the correct value to send to the speed register. The manual says: The SPEED register contains the current motor speed, expressed in step/tick (format unsigned fixed point 0.28). In order to convert...

Resolved! STSPIN32F0A BLDC Sudden motor stops

Posted on March 10, 2018 at 13:49Hello,I am in the process of developing a custom sensored BLDC driver board using STSPIN32F0A IC. The motor used to develop this board is very small and uses less than 10W of power. For now, the lab power supply is s...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.