2018-04-02 7:41 PM
The L9907 datasheet states that I/O is 3.3V logic compatible. It also states that I/O pins can withstand voltages up to 35V in the 'Absolute Maximum Ratings' section on page 17. I was wondering if it were wise to have a PWM 5V logic signal coming into the L9907 3-Phase Gate Driver interfacing with 5V PWM from MCU.
2018-04-02 7:43 PM
For some reason, the last sentence wasn't finished for some reason: 'I was wondering if it were wise to have a PWM 5V logic signal coming into the gate driver.'
The reason I ask whether a 5V logic signal will be permissible is because the 35V rating is for an absolute maximum value and is not specified as a recommended operating condition. Sorry if this is a silly question.
2018-04-06 7:57 AM
Hello Tom,
no problem in having 5V signal to L9907 logic input.
Best regards
Stefano
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.