Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

POWERSTEP01

I am developing a control system, for an industrial doser, for this I use a stepper motor, of 5.6amp, 0.5 ohm, 3.6mh and a KE .233.I have all the system implemented, hardware and software.To tune the engine I used the EVLPOWERSTEP01 development tools...

Juanfra by Associate
  • 924 Views
  • 0 replies
  • 0 kudos

Wireless power receiver STWLC03 specifications

I would like to know the following specification of STWLC03.I tried to find the STWLC03 datasheet, but I could not find it on your wave site.Would you please let me know them.  ・Input AC voltage Maximum rating  ・Output voltage Maximum rating  ・Digita...

Fumio.N by Associate
  • 784 Views
  • 0 replies
  • 0 kudos

How do I get my motor to spin?

I have a BLDC  4 poles motor with a rated voltage and current of 36V and 7A. I followed the instructions on the get started pdf for the STEVAL-SPIN3201 board, tried to change de start-up parameters and I can't get my motor to spin.

JFons by Associate
  • 663 Views
  • 0 replies
  • 0 kudos

CURRENT MEASUREMENT BY 2 SHUNT RESISTORS

Hi All,Having some doubts regarding the current sense.When using dual shunt current sensing technique, we have 2 current sense resistor at the Phase A and Phase B inverter legs.The 3rd phase current can be calculated in code.But ,my concern is regard...

RTHOM.17 by Associate
  • 970 Views
  • 0 replies
  • 0 kudos

Designing a battery charger with solar harvester

Hello,I am looking for a charger IC for a medical application with the following characteristics and was wondering if you could advise me.General The device is a low power device with a battery and a solar panel. 5V and 3.3V are required for the appl...

Problem with 2 bits ABS_POS

Hi,I'm using two L6472 with kinetis processor.Everything seems to be ok, except for ABS_POS ( absolute position register). When i read value with getparam(abs_pos) 2 bits stay all times at 0 and obviously data are corrupt.In first time, I think It's ...

JRost by Associate
  • 691 Views
  • 0 replies
  • 0 kudos

HVLED001A - Over voltage ishue

Designing an 80W power supply based on HVLED001A for 40V out at 2Amp. The issue is at lower loads it shots up to 60V. loads greater than 1 Amp it drops down to 40V. the layout is based on the edesign suite by ST., in addition, the Cclp, RCLP, HVLED00...

SRata by Associate II
  • 2724 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.