Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

We are using EVALPWD13F60. We are unable to make motor turn on.

We are using EVALPWD13F60. We are unable to make motor turn on. While we give pwm(10KHz) to HIN1 and LIN2 with different duty cycles by putting LIN1 and HIN2 as low , we getting 6 V as output. When we give HIN1 and LIN2 full time high voltage is drop...

APadm by Associate
  • 981 Views
  • 1 replies
  • 0 kudos

Using STEF01 UVLO below recommended voltage 8V?

By resistor calculation and also by given graphic it is possible to adjust UVLO voltage as 4.5. However, in datasheet, it is written that using UVLO below 8V is not recommended. What happens if UVLO threshold used as 4.5 V?

SErbo by Associate
  • 780 Views
  • 0 replies
  • 0 kudos

Resolved! How do I get 60W profile from STUSB 4500 ?

So i need a sink setup with the standalone stusb 4500 but i can not find examples on how to make a 20v 3a setup for negotiation. Anyone who could bring some light into this ? Maybe you have a schematic you could share so that we all can find or is it...

Spice Model for STW15NK

Hi,I tried to use the spice model for the STW15NK (.subckt) but it dosn't work with LTspice.I imported the .subckt with LTspice without any error.But the FET don't torn on/off with the input signal on Gate.Any known issues?thanks,Martin

VNH5019A-E gets damaged while hot plugging with motor, as we disconnect the motor when it is being driven by this H-bridge. Kindly find attached schematic. We require your valuable feedback in this regards. Thank you very much.

We are using VNH5019A-E to drive an actuator. We have followed all the schematic mentioned in evaluation board of VNH5019A-E for the system. We have a case when we have to disconnect the motor while this H-bridge IC is driving it. In this scenario of...

0690X000006DSZ5QAO.png
AVyas by Associate
  • 843 Views
  • 0 replies
  • 0 kudos

STSPIN240 - never get fault interrupt

I'm driving a small engine and almost everything works well. Running current is about 13mA and 80mA at the end when it is directly driven. When driving with the STSPIN240 and the actuator come to an end the driver's output go into switch mode and lim...

TLjub by Associate
  • 673 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.