Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Can I use STD25N10F7 to replace STD15NF10 ?

Hello,I appears that STD25N10 is designed to a replacement for the STD15NF10. Do you confirm?Do you have any comparisons or recommendations about external gate resistors when this device is used in a three phase inverter application? NOTE: This quest...

Auxiliary winding and Self-Supply Viper16

What are the benefits of powering Viper using Auxillary winding and not self-supply?Can I power using VIPer self-supply for my Flyback converter SMPS design?How will it affect the working of the Viper?

RKara by Associate
  • 671 Views
  • 0 replies
  • 0 kudos

Data Sheet Missing for STL18N65M2

The Data Sheet of STL18N65M2 is missing.On mouser.com and digikey.com I found only a preliminary data sheet without graphs.I need the graph of Rdson to check, if this MOSFET fits my application.Please update the data sheet.The link on your website is...

Does IHM08M1 can drive a BLDC motor(250W) with heavy load?

Dear All,​I use a IHM08M1 with FOC control to drive a 250W motor. Motor can ramp up with light load and spin well. When the load was increasing to 90KG, motor failed to start up. After adjusting startup parameters and control mode(torque / speed), it...

AChen.17 by Associate
  • 1952 Views
  • 4 replies
  • 0 kudos

How to get the energy value from STPM32

Hello,I am using STPM32 as my power sensing IC. In this I am accessing the register 54 to get the energy value. when I access the register 54 it gives me a hex value of 0x52F8FFFF. I dont know how to interpellate this to get the energy value. Please ...

L6564 used to BUCK controller, the buck output voltage is not set-point voltage at startup, and L6564 control logic is incorrect

L6564 used to BUCK controller, the buck output voltage is not set-point voltage at startup, it's output is equal to input as duty cycle =1, please help to resolve it, thanks.the below is waveform and buck circuit, CH1 is output voltage B+, CH3 is buc...

0690X000008A6NpQAK.png 0690X000008A6NkQAK.png

Why is heating up L6230 chip (on IHM07M1 expansion board)

I have a Nucleo-F302R8 board with X-Nucleo-IHM07M1 motor driver.When I run the motor (using my sensorless algorithm, PWM frequency is 20kHz) the L6230 chip is started to heat up and the temperature of the chip has very fast increased.In the L6230 dat...

DBake.18 by Associate II
  • 732 Views
  • 0 replies
  • 0 kudos

the F302 project example of X-CUBE-SPN8 doesn't work

Dear I try to flash the example image which is located at the following path"STM32CubeExpansion_SPN8_V1.0.1\Projects\Multi\Examples\MotorControl\Src"to development board and using six-step to start motorbut the motor doesn't startup , check the failu...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.