Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Hi. I designed the power conversion circuit with A6986.After soldering of this pcb, I powered 24V on power line.And the VIN pin(#15) was damaged.I have no idea what is the problem.when I design the circuit, I consulted the manual, and eval. board...
Hello, I have switching power supply with some IC from STMicroelectronics with ST eZ12042 marking on them but i can't identify them and find datasheet. I will be grateful for any helpThanks in advance!
Hi,i am desining an inverter using STM reference design AN3095.i happen to notice that the bridge rectifier section has been implemented using two fets and two diodes.Why is that so?What is the significance in such a method?Why din't they use four di...
Hi,We have built devices that run on batteries and serve a specific task. For the future we also want to offer a wired solution, for better user experience and more features, that would drain the batteries faster. Since the wired solution already re...
I'm using L6474h with X-CUBE-SPN1 Version 1.10.0. I think there is a bug with the X-CUBE-SPN1 library.Step motor movement is delayed for a few seconds if the speed is adjusted more than two times (x2) of the previous speed. There is no problem if the...
[I used a translator.]Hi,I run the motor in "drv8835 Fast DK Mode".The following waveform appears on the oscilloscope.When the pulse is low, about 6~7V is outputIs it working correctly?Is it normal not to fall to 0V?When operating in Slow DK (phase ...
I use the ST EVAL 6470 driver board to control a stepper motor in my tracking system! I need to send out some fairly "fast" sign changing commands! This seems to make the control board unstable! The Busy/Sync led starts flashing and starts an unwante...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.