Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STLA02, In the datasheet I have seen the resistor value is calculated as per for feedback voltage.How I can control the booster voltage.What is the Voltage at the Vout pin.

STLA02, In the datasheet I have seen the resistor value is calculated as per for feedback voltage(200mV).How I can control the booster voltage.What is the Voltage at the Vout pin.How the resistor value is calculated.Let me know the feedback for the s...

VVelu by Associate
  • 596 Views
  • 0 replies
  • 0 kudos

Time over of L6924D Charger

Hi all,I fixed 3 hours fot the maximum charge time.The question is : when Tmaxch =0, the condition will be IND FAULT so the circuit restart the charge or user who will do that ?Thanks and best regardKhalil

CKhal by Associate
  • 740 Views
  • 1 replies
  • 0 kudos

Do you have a Windows 10 version of STEVAL-IHP005V1_Setup?

We have laptops running Windows 8 and Windows 10 and on both we installed this software STEVAL-IHP005V1_Setup.exe and the software crashes every time. We set the compatibility mode to Windows 7 and still the same issue. Unable to use this software to...

NNage by Associate II
  • 712 Views
  • 0 replies
  • 0 kudos

STM6600 voltage divider on VCC for high voltage applications

Hi, I'm evaluating the STM6600 on/off controller. My application has a 2-series LiPo battery with a voltage range of 6 to 8.4V, so I need to put a voltage divider before VCC as described in AN3271. The calculations for the divider provided in that do...

JPent by Associate
  • 748 Views
  • 0 replies
  • 0 kudos

"eDesignSuite" of Interleaved PFC Specifications

Helo,I have recently bought a STEVAL-IPFC01P1, to evaluate de STNRGPF01 controller.I want input voltage spec to 90-265VAC at 47-63Hz rangeHow can I change it?I'm tried the following way... 1) Interleaved PFC Specifications clock 2) "Mains Wide Range ...

Kdaeg.6 by Associate
  • 740 Views
  • 0 replies
  • 0 kudos

STSPIN32F0 and STEVAL-SPINS3201 Problem

Hello friends,I made a custom STSPIN32F0 board , copy all sames STEVAL-SPINS3201 except STM32F103 side ,We upload default software from motor library and system works well in EVM SPINS3201 but when we upload same software to our boards , there is no ...

Converting ADC Bit Value to q1.15 Current in "per Unit"?

Hi,I'm reviewing a code for PMSM motor control with FOC. The library used is an older one and described in UM0492 "STM32F103xx permanent-magnet synchronous motor FOC software library V2.0" (attached file)I'm wondering how the software know what curre...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.