Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

L6566B reset indicating shorted

We designed an AC / DC power supply with the L6566B with the help of the eDesign tool. We manufacture a 5-piece pilot lot and are encountering a problem with two parts that do not start the L6566B.Taking some measurements we realize that at pin 5 (VC...

JunexR8 by Associate II
  • 640 Views
  • 0 replies
  • 0 kudos

L6566B reset indicating shorted.

We designed an AC / DC power supply with the L6566B with the help of the eDesign tool. We manufacture a 5-piece pilot lot and are encountering a problem with two parts that do not start the L6566B.Taking some measurements we realize that at pin 5 (VC...

JunexR8 by Associate II
  • 744 Views
  • 0 replies
  • 0 kudos

FOC Motor Control: Speed Mode Control Behaviour

Hello EveryoneI'm using FOC Motor Control to spin three differents motors. It works quite well, but I'm attemping to obtain more power from motors, and I'd like to know how to do it.With a potentiometer, I vary speed reference and system works fine. ...

STNRGPF01 Firmware Loader doesn't detects COM Ports !!

I've designed a control board with STNRGPF01 3Level Interleaved PFC Controller. After creating hex file by eDesign Suite, i want to load firmware to stnrgpf01. But STNRGPF01 Firmware Loader doesn't detect com ports. There is no com port on loader too...

Source code

Application note for sensored BLDC Motor C code for stm8s for STV.

VSaha by Associate
  • 796 Views
  • 0 replies
  • 0 kudos

EVAL-VNH5019 motor driver problem

Hello,I’m using EVAL-VNH5019 to control TEC element, and connect it as datasheet and databref in the link below, the power supply connected to the driver is 20 VDC and PWM used (15625 HZ) but the problem is when I applied 50% duty cycle on PWM pin I ...

AAlha.6 by Associate
  • 744 Views
  • 0 replies
  • 0 kudos

We are using L7805CV , Input voltage = 30V output expected = 5V with 100mA of current requirement But we are getting 7.5V, the L7805 which is not correct,may know the reason?

We are using L7805CV ,Input voltage = 30V output expected = 5V with 100mA of current requirementBut we are getting 7.5V, the L7805may know the reason?according to datasheet input voltage is 35VCurrent supplied to the micro controller board and output...

BGowd.18 by Associate II
  • 1174 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.