Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DMcDo by Associate
  • 509 Views
  • 0 replies
  • 0 kudos

We are using L7805CV , Input voltage = 33V output expected = 5V with 20mA of current requirement But we are getting 7.5V, the L7805 may know the reason? according to datasheet input voltage is 35V

Current supplied to teh micro controller board alone,it is nowahere connected,Still 7805CV not able to deliver the 5VPlease find the attached circuit and let us know please let me know why this circuit is not working or let us know the input voltage ...

BGowd.18 by Associate II
  • 5256 Views
  • 8 replies
  • 0 kudos

Resolved! How to fix the power consumption of STC3115?

I have a design with STC3115AIQT as in picture:VBAT and GND are connected to positive and negative terminals of a Li-Ion battery, respectively.When the device is powered-off 3V_L is connected to GND. In this condition VIN pin is sinking 3mA of curren...

0690X000008w2F0QAI.jpg
Raghu by Associate
  • 1430 Views
  • 1 replies
  • 0 kudos

Setting up STEVAL-FCU001V1

Hi.I am a bit confused how to set up the STEVAL-FCU001V1 kit. Is there any kind of tutorial on how to load a firmware onto the board? I've got a STLINK-V3SET and a STLINK V2. Where do I have to connect the Powersupply and the SWDIO and SWCLK from the...

5V 1A power supply using ALTAIR04-900TR

i have made 2 pieces of 5V 1A power supply using ALTAIR04-900TR  as per the circuit design in eDesignSuite.Now as i power on one of them it blow the fuse and rectifier in AC input. i tested for any sort of short circuit but i did't find and again i ...

MVERM.4 by Associate
  • 719 Views
  • 0 replies
  • 0 kudos

Voltage drop at motor input

Hi everyone. I'm new to motor control and have some problems with my robot. We are designing a three-wheeled omnidirectional robot which should bare and transport weights about 10 kg. We use Pololu 12V DC motors which has a stall torque of 8.5kg-cm....

N ORhan by Associate III
  • 763 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.