Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

yqn by Associate
  • 714 Views
  • 0 replies
  • 0 kudos

Oscillation in STW88N65M5 transistors

We are testing a 300kW inverter prototype, consisting of 12 modules of 25kW, connected in 3 phases of 4 modules in parallel.Each 25KW module has a full-bridge exit stage of 8 STE88N60M5 transistors, in parallel to 2. The sineworm modulation of the PW...

Problem in stm32f103c8t6 while running motor on load condition

Hi friends, I am driving bldc motor using stm32f103c8t6. And i measure the rpm of the motor using the hall sensor pins. While running motor on no load condition....Motor runs good .Rpm is also measured and i monitored in keil debugging session, which...

svraj by Associate II
  • 5271 Views
  • 5 replies
  • 0 kudos

L6566B reset indicating shorted

We designed an AC / DC power supply with the L6566B with the help of the eDesign tool. We manufacture a 5-piece pilot lot and are encountering a problem with two parts that do not start the L6566B.Taking some measurements we realize that at pin 5 (VC...

JunexR8 by Associate II
  • 687 Views
  • 0 replies
  • 0 kudos

3-Phase Motor

Hello,I ordered STM32F769I-EVAL and IHM028V2.BLDC motors, mc_startmotor, mc_stopmotor and so on I was using commands using atollic. Can I also do these commands on a 3-phase ACIM on the atolic?

trgyada by Associate II
  • 831 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.