Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
I want to use STGB8NC60KDT4 IGBT, 15 A 600 V, 3-Pin D2PAK (TO-263)in a motor controlpower bridge, The bridge will be running at 300VDC and about 3-5 amps. At this power there will be 6-12 watts dissipated in the IGBT.I would like to cool them by scr...
Is external protection needed?And what type off protection if it also should be able to handle EMC Burst and Surge pulses?
compensation pin and ground pin is shorting ?WHAT ARE THE POSSIBILITIES TO FAIL THAT 2PINS ???
I am trying to drive a 3 digits - 14 segments display with the STP16CP05, but I cannot find any information related to multiplexing this component.Does someone already did this ? Thanks
hi i use your product SG3525 for Solar inverter (input-dc 12v , out put -110v ac 60hzcould you recommend me how to use transformer for step up tr(T1)how to calculate core size, coil thickness and turns for primary, and secondaryalso i hope to know i...
Chapter 8.5 says write the register value as two bytes (Low and High), but all pictures and descriptions later sends only one byte for the register value. Whats correct?If I send START ADR(WRITE) REG START ADR(READ) VALUE STOP the ADR byte is acknowl...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.