Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STEVAL-POE001 not engaging when connected to 802.3AT PSE

I purchased a STEVAL-POE001 evaluation board for testing. Connected the board to several PSE units including an injector and a switch that supports 802.3AT. The board and the PSE LEDs flash momentarily but will not fully engage. I do not have any...

BBarn.1 by Associate
  • 1203 Views
  • 0 replies
  • 0 kudos

Port SPN3 motor-control examples to DK2?

We are considering using a combination of the stm32mp157 and several powerSTEP01 devices in a system with multiple stepper-motors.The X-NUCLEO-IHM03A1 plugs into the -DK2 just fine, but the SPN3 examples only work on the F0xx, F3xx, F4xx, and L0xx se...

Using the VNHD7012AY development board to run a brushed 12V motor, I have trouble at initial startup trouble that appears to be a problem with the fault circuitry.

Picture #2: (Current waveform) Operation with resistance added to OUT linePicture #1: (current waveform) Picture when motor does not start Regardless of what values I install for gate resistors (0, 475, 1100 ohm), Vref resistors (8-40K) adding ext fi...

0690X00000DYokxQAD.png 0690X00000DYokiQAD.png
PCond.1 by Associate
  • 1065 Views
  • 1 replies
  • 0 kudos

Max load on output of STEVAL-ISC005V1

Hello, What is the max load I can put on STEVAL-ISC005V1? I mean, I try to load 100W on PD03, setup to 20V/5A, with an electronic load but something burn on the evaluation board, I thing I make something wrong. Could somebody help me with this topic?

DIsel.1 by Associate
  • 766 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.