spice models for ST1L05CPU33R
Hi , We are using ST1L05CPU33R in our Design. We need spice models for ST1L05CPU33R. If you have this. Could you Please share with us.Thanks & ReagrdsKranthi
Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Hi , We are using ST1L05CPU33R in our Design. We need spice models for ST1L05CPU33R. If you have this. Could you Please share with us.Thanks & ReagrdsKranthi
Circuit which i am designed is attached. pls verify this circuit.I want to know whether, can i program this board(designed circuit) with st NUCLEO-F072RB board by taking connections SDA and SCL pins out and connect it to st development board.Can i us...
I am trying to understand the max rpm limitation. I previously thought that the theoretical max speed would be calculated by Kv * battery voltage. But in any case the real max speed at no load is a half of expected.I use a STEVAL-ESC001V1 at 18V with...
Dear All,I've a problem with my step-down regulator L7985A.On power up, the DC / DC is activated when the ENABLE pin reaches about 880mV, while on the datashhet it is reported 1.2V as the ON threshold.Can you explain to me what this difference is due...
HI Sir, May I ask you for the help due to the quality issue of TIP147, functional fail,Customer would like to known what the problems and want to get analysis report,Attached is the picture for the component, what the information needed to provide th...
Hello, we have a L9907 evaluation kit and we are trying implement the software to get L9907 to run. We have some problems we need support for:we supply the board at 24V and are using the VBAT_Scal circuitry to scale down the voltage on the VB pin, bu...
Our BLDS motor becomes warm/hot at no load, at room temperature. In our application the surrounding temperature is more then ambient up until 55°C. Any addition heat that we generate inside the motor will cause the motor to quickly overheat, with pos...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.