2019-01-05 12:40 AM
Circuit which i am designed is attached. pls verify this circuit.
Solved! Go to Solution.
2019-01-07 8:00 AM
Hello,
thanks for your schematic. I reviewed with the application team and there are indeed a couple of feedbacks we'd like to share with you. Would you mind sharing your email address through direct messaging? (click on my name from this discussion and then MESSAGE button).
To answer you question:
Benoit
2019-01-07 8:00 AM
Hello,
thanks for your schematic. I reviewed with the application team and there are indeed a couple of feedbacks we'd like to share with you. Would you mind sharing your email address through direct messaging? (click on my name from this discussion and then MESSAGE button).
To answer you question:
Benoit
2020-03-27 11:03 AM
Hi,
I have bought a new NUCLEO-F072RB and I have used the CubeMX software to create a project with the default settings, when I build and debug the code I am able to flash it but when I debug it, it always fails on the SystemClock_Config. I have then bought a new board thinking there previous board was faulty but even the new one does the same thing.
I have previously used the NUCLEO-F302R8 and NUCLEO-F676I and generated a similar project for them where I easily achieved a simple LED blink project before proceeding with the actual purpose of purchase. This time I have bought 3 NUCLEO-F072RB boards and none of them seem to work. When I first connect them to the laptop they have the default LED blink code where the LED changes dutycycle at every input of the user button (blue) but when I generate the project with CUBEMX it never reaches the "while" loop as it keeps failing on the SystemClock_Config function.
I Would appreciate any help, Thanks in advance.
Kind Regards
Manpreet
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.