Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Which debugger/programmer is recommended for STEVAL-HKI001V2 ?STLINK-V3SETSTLINK/V2ST-LINK/V2-ISOL
Hi there,I am interested in automatic radiator control valves (energy harvesting or batteries powered). Do you have any suggestions?Thank you!Best regards,Oskaras
Hi, what is the behaviour of the IRQ-Lines of the LED1202 when connected wired-OR as in chapter 6.2 of datasheet (i.e. clock synchronized 1x Master, 2x Slaves)? I want to use SHFT=1 on all 3 devices.As per datasheet, the update of the PWM - registers...
I've set up the POWERSTEP01 driver in voltage mode, which works nicely. Now I want to use the sensor less stall detection feature to implement sensor less homing. How must the stall_th and also the ocd_th values be dimensioned for this to work correc...
The ENABLE/FAULT pin delivers back a voltage that provides the part status (Table 6 of the DS).It is said that OK = 5V; thermal fault = 1.4V; power protection = 0V.As this pin must be directly connected to a 3.3V FPGA pin, I made some measurements wi...
Hello,I have the x-nucleo-ihm08m1 board and looking into the schematic I do not see the potentiometer R42 in there.I bought my board recently from mouser.The schematic i downloaded from the web page of the board (attached).Thanks in advance.
Hello All, I'm developing 48Volt 700Watt BLDC Motor Controller Using STM32 Controller. I didn't use STM Motor Control Workbench Tool for this Project. I developed my own library and source code for this project. When motor is running initial spikes i...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.