Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STEVAL-ISV020V1 - Absolute value for input voltage

Hi, In the evaluation board of SPV1050 (STEVAL-ISV020V1), it is mentionned that the maximum voltage from the PV cell (VMP) is to be equal 9V, but there is no indication about the absolute values that I can be supported without damaging the board. I'm...

GAbi .1 by Associate II
  • 1378 Views
  • 3 replies
  • 0 kudos

Resolved! Motor driver

HelloI am using in my project both brush and brushless motor. My circuit works from 1 cell lion and have dc-dc step up to 6v for my motors.My sensorless brushless motor part number is : https://www.maxongroup.com/maxon/view/configurator/BOM:ECXZ08M1V...

My questions about EVAL-L9963 are following: Does it work with NiMH battery chemistry? Can it support each individual channel voltages of up to 14.4V nominal voltages (voltages may vary as high as 18.8V)? Can it perform passive and/or active balancing?

I am working on BMS type of system that will recondition, balance, and maintain NiMH HEV batteries. I'm considering to use L9963 IC and its accompanying evaluation board EVAL-L9963 for my prototype. My system consists of nickel-metal hydride battery ...

0693W000005BwmPQAS.png
VVasy.1 by Associate
  • 1028 Views
  • 2 replies
  • 0 kudos

Resolved! EFL700A39 - rechargeable solid state lithium thin film battery

Hello, this message is addressed to ST employees, if you could please send me additional information not present in the datasheet.I'm using the EFL700A39 rechargeable solid state lithium thin film battery. I'm trying to figure out the state-of-charge...

GAbi .1 by Associate II
  • 1346 Views
  • 3 replies
  • 0 kudos

Resolved! STEVAL-ISV020V1 resistors in the datasheet and in reality

Hi, I don't know if other people have had this problem.Actually, in the datasheet of the STEVAL-ISV020V1 is mentionned that:R1 = 10 MohmR2= 1 MohmR3 = 5.6 MohmR4 = 6.2 MohmR5 = 500 KohmR6 = 2.7 MohmHowever, when I received my evaluation board, I meas...

GAbi .1 by Associate II
  • 1534 Views
  • 3 replies
  • 0 kudos

UL certification of STEF05P electronic fuse.

Hello, Can you provide me the details whether the STEF05P electronic fuse is UL certified or not?I need to use the component in a device where the safety related components should be UL certified.Awaiting response.Best Regards,Sushant Rajbhar

SRajb.1 by Associate
  • 1034 Views
  • 2 replies
  • 0 kudos

Resolved! IBUUI.inf driver fails to install when using IBUUI Board Updater

Hi,I am trying to use a STEVAL_PCC009V2 board connected to a EVAL6474H board to drive a stepper motor.When I run the SPIN eval software I get a notice that the firmware is not the latest and I need to update it. I just ordered the board, but it shows...

DSabo by Associate III
  • 1188 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.