Resolved! Marking Information LD1117S50CTR
we have purchase this item LD1117S50CTR recently, Can i get the marking information, our QA department is asking us provide information to process production, thanks.
Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
we have purchase this item LD1117S50CTR recently, Can i get the marking information, our QA department is asking us provide information to process production, thanks.
Hi,I'm testing a simple flyback converter using the STCH03L. All seems as expected, however I can not seem to get the IC to detect an overvoltage condition. To conduct the test I am simply shorting out the optocoupler. When I look at the ZCD pin the ...
Hello,I'm trying to discharge the solid state thin film lithium battery EFL700A39, with a discharge current of 0.7 mA, in the aim of reaching a state of charge of approximately 20%. Actually, the problem is the significant difference of voltages whe...
The datasheet (https://www.st.com/resource/en/datasheet/spv1050.pdf) mentions that the STORE voltage during initial start is charged through a charge pump, when in boost configuration.However, when I set my load to 0 V and input to 2 V, it sure seems...
I have an SPV1050 configured as follows:R4 = 6.2MR5 = 1MR6 = 3.9MVeoc = 3.5VVuvp = 2.78VThe device is configured for boost mode with MPPT set to 75% and Vin = 2V. The device works as expected, except that it will only draw the full specified 70mA cu...
I found this two in market help me to find out original one, also tell me to check visually that which one is original?
i need a dc-dc step down power supply where the input varies from 45-55volts and required output of 5volts and 10amps
Hello everybody,I need a power conversion DC-DC 24V to 3.3V. So I went to eDesign suite who recommendend me the following architecture:I reproduced it in my design: I produced the board, and when I apply 24V on the input, I obtain only 0.9/1V on the ...
HIUsing eDesignSuite I can not design more than 600mA Buck. Is it impossible? and I want to use Htype but eDesignSuite dose not support. Please explain about this problem.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.