Qi-compliant inductive wireless power receiver for 5W applications
Is it possible to configure inductive wireless power receiver without using GUI
Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Is it possible to configure inductive wireless power receiver without using GUI
Hi,I see that STWLC68 has a 32-bit 64 MHz ARM Cortex microcontroller core. How can I program or debug this device using STM32CubeIDE. I'm not able to create a project with this device.gaston
Hi,In the SPV1050 datasheet, in the Electrical characteristics section, the VMPP voltage range is defined as 0.075V to VUVP - 0.1V. I do not understand why VMPP is limited by VUVP. In buck-boost configuration, certainly the input source's maximum pow...
Hi everyone,I am using two mosfet as a switch (in order to open or close a contactor, turn-on or turn-off some PCBs, etc, not high frequencies are required), one high side mosfet and one low side mosfet. I want to control them with the L6395 driver.W...
Hi, I am designing an application using the SPV1050. I am not using the LDO function, and am only using the SPV1050 for charging my battery.I have tied LDO1_EN and LDO2_EN to ground. Can I safely ground the LDO1 and LDO2 pins as well in this configur...
Apart from the V_RMS, I_RMS, power and energy (all aggregated), is it possible to output the ADC readings real time over SPI? I am looking to get 8k samples of I and V out of it. As of it was a pure ADC, with the filtering, but without the calculatio...
Hi,Please help with the "TL431CDT"There is "H" symbol on the marking code (431CH)What does it mean?There is nothing is the datasheet (marking 431C without H).Best regards and thank youLuca
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.