Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Dear ST community Hello,I am using the STGIB15CH60TS-L for motor control, I have a question about the schematic in ST documentation.Could you clarify to me please about the switches sw7, sw5, and sw6 used in the low side transistors for current measu...
Dear ST team,I want to design an SMPS circuit with the following specifications:* Input can be either 33-265 VAC or 48-375 VDC (ultra-wide input)* Multiple DC outputs1.output : 24V with 0.7 A2.output : +10V with 0.8 A1.output : -10V with 0.8 ...
I’ve build 5 boards using PM8804 and only one board seems to regulate the VC (Output of the internal high voltage start up regulator) according to the datasheet where the high voltage regulated drop below 6V when it detect auxiliary power detected hi...
I noticed the pads of these pins are very small. I'm a bit worried this is critical with high-current thoughput. For my application current peaks might exceed >5A for couple us. Pads like GND, VS and OUT are very large in comparison..
Using 2xL6491 in a full H-Bridge inverter for a PMDC motor, PWM switching frequency is 32kHz. With the smart SD threshold set low to verify the functionality, we see what appears to be skipped PWM pulses most likely due to the shutdown system blockin...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.