Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Hello, I have an IPM10F and try to switch on the gate, so I can measure a current on the Output U. My Problem is I measure nothing.I put a constant 3.3 Voltage to the Gate-Pin A-High. On the Output (U) I connect a resistance to override the LOW-Switc...
I design a pulse output circuit using the L6389E. I'm looking for the L6389E spice model, where can I find it? Thanking you in advance.
The product's part number is "VNL5030JTR-E". They had different levels of ecopack. One is ECOPACK 1, another is ECOPACK 2. I found the website shows the product is Ecopack1 in May 25, 2021. But now the website shows the product is Ecopack2. Coul you ...
I'm experiencing issues when I talk to other devices on the SPI bus and then talk to the STPM34.I've confirmed the startup sequence of the STPM34 is correct, and if I never talk to the other device(s) there is no issue with the STPM responses.However...
Hi. I am interested in using the STEVAL-IPMM10B evaluation board to drive a BLDC motor with the voltage rating of 50 V. The evaluation board user manual says, it works for 125-400 VDC. Is there any way I can use this board for lower voltages? Thanks.
Hi all,We're on a project which involves WPT, so we selected the STWLC68 component. We bought the evaluation board STEVAL-ISB68WA and we tested it with the steval-isb045v1 base, as indicated. Once verified the functionality and the tuning procedure, ...
Dear Support,Please advise if the DC is shown in the topside marking of part number L7987LTR?Kindly advise how to read DC. Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.