Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Hello, please help, I can’t identify the SMD component and its datashit, ST G AC GP 752.
The part number is std120n4f6. The framework of DC 2045 is inconsistent with those DC after 2101.I want to know if there is a PCN about this problem during 2045 and 2101.
3D STP model is need to run thermal simulation. Detailed POA is embedded in the datasheet. Package DFN4 1x1mm.
Full note below:"At last, a resistor RGK between gate and A1 (this terminal is still also called “cathode�? as a reference to a Triacformed by two SCR) finalizes the drive circuit. Its purpose is to reduce spurious triggering of the power Triaccaused...
I have to buy three STEVAL-DPSLLCK1 in order to make three Dual Active Bridge bidirectional DC-DC converter prototypes.I need to add some functions to its fw. It is the source code available.RegardsPaiardi Giuseppe
The Firmware package provided for the STEVAL-DPSLLCK1 LLC kit only contains binary files. Where can I find the IAR project files?
Hello ST Team,we are currently designing a product where we want to have an output pin with ~0.5-1A current capabilty and the ability to switch this output to High (12V - 48V depending on product variation) and LOW (GND). For this we plan to use a du...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.