Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I'm using the STC4054 Li-ion single cell charger in a design, the CHRG pin is supposed to have a weak pull-down when not charging but the current drawn is higher than specs

In the STC4054 datasheet, it says the CHRG pin is supposed to have a weak pull-down of max 35uA when no battery is connected yet. However, with a 4.7Kohm pullup from that pin to 3.3v, I measure a 1.2v drop, which indicates about 250uA of current. Wit...

PVaca.1 by Associate
  • 1292 Views
  • 2 replies
  • 0 kudos

Help with nucleo board and pca9685 servo board

Hello everyone,I came here looking for help : I'm doing a project for an intership where i have to create an hexapod robot basically from the ground up, with particular interest in the electronics and programming part.As a main microcontroller, we ar...

FGuns.1 by Associate II
  • 4846 Views
  • 3 replies
  • 0 kudos

Resolved! Confusing about behaviour of L6470 MOVE(dir, n_step) command

HI folks!,I'm here because of I am a little bit confused about the behaviour of MOVEcommands sent to a pair of L6470 devices connected in daisy chain.The problem that I'm facing happens also if I sent the commands only toone motor.In our project both...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.