Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! About VNL5030JTR-E

Thank you very much for your help.My name is Ichikatai, Designe Engineering Department, NIKKI CO.,LTD.Regarding the VNL5030JTR-E productI believe that high melting point solder (lead 85% or more) is used in the semiconductor chip part as an exemption...

Ichi by Associate
  • 1432 Views
  • 1 replies
  • 0 kudos

exposed pad

“What could happen if the exposed pad of the LD39200 is not properly grounded? Could it affect its functionality?Is there any limitation regarding the reflow temperature for the LD39200, considering that everything seems fine initially but only 0.4 V...

Sin título.png
rmessino by Associate
  • 1387 Views
  • 1 replies
  • 0 kudos

Driving GaN FET Transistors with the STDrive101 / STSPIN32 range

Hi,Is it possible to use a STDrive101 to drive a GaN FET give the typical 6V Vgs max rating of these devices?I read the datasheet reference to 5.2.2 Externally provided gate driver’s supply voltage to see if we could home how reduce the 12V LDO to sa...

Screenshot 2024-02-15 162405.png
CDill.2 by Associate II
  • 1095 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F405 behavior when VCap pins aren't connected

Good morning,I'm using STM32F405 for my embedded project and this PCB version showed itself a real MCU killer... So far, it has already burned 4 MCU. Here's my situation. It's not my first time designing using an STM32 (I've already used STM32F103), ...

Agatti by Associate
  • 3344 Views
  • 4 replies
  • 2 kudos

Different reading on shunt depending on motor direction

We have based this board off of  EVAL-L99H02QF.We are having a difference in current reading on CSI2. We have 2 shunts, and the one that goes to GND R38 in my picture has a different reading whether motor is going one direction or the other. We canno...

Joshcm by Associate
  • 1326 Views
  • 1 replies
  • 0 kudos

PowerStep01 step clock mode, maximal acceleration

I have a motor that is capable of of an acceleration of more than 1'000'000 steps/sec^2. However, I cannot this high acceleration because the max. acceleration the internal motion engine of the PowerStep01 allows is 59590 steps/sec^2 (ACC Register, S...

pf8645 by Associate II
  • 939 Views
  • 0 replies
  • 0 kudos

Resolved! WLC poller/listener development boards or and app notes

I am lost and confused between the wireless charging topic when it comes to development boards. Which ones should we order in order to test the working principle of the wireless up to 1W charging?Is ST25R3911B-DISCO the one to use as the WLC-Poller? ...

Val by Associate
  • 3808 Views
  • 4 replies
  • 1 kudos

Resolved! Need help IDing a TVS

I have a PCA with a blown TVS. The markings are: ST e3 G3BA◇YZ521I've seen TVS datasheets with markings starting with 3BA, but the diamond symbol is throwing me off. Can you assist?

IMG_2239.jpg

Disabling open load detection in L99LDLH32 driver

Hi, I am using the L99LDLH32 driver in an application in which some of the output pins of the driver are in open load, the problem is that in this way an open load fault is generated by the driver, deactivating all the output channels. Is it possible...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.