Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ALED1262ZT burn OTP I2C address

We've developed prototype board with 3 pcs AL1262ZT (https://www.st.com/en/power-management/aled1262zt.html). As a 'fresh device' it has 0x40 I2C address and it's need to specify unique addr (0x42, 0x44, 0x46) by burn OTP register. Our procedure: 1. ...

owiec by Associate
  • 1211 Views
  • 0 replies
  • 0 kudos

stwlc38 firmware download issues

We use wireless charger RX IC stwlc38, though we tried to write firmware which provided by the link https://github.com/STwirelesscharger/STWLC38_NUCLEO_L476RG, but we met the CUT id mismatch during firmware writing via I2C interface and then the F/W ...

daveoh by Associate
  • 1406 Views
  • 1 replies
  • 0 kudos

STWLC38: GUI connect No response

Hello, I have a custom board with a STWLC38JRM. Everything was fine and I was able to flash it with STSW-WPSTUDIO v1.8.4 through the dev board STEVAL-WLC38RX and FT_SDA/FT_SCL/VBUS/AGND pins. I try to make some test and I disabled internal overtemper...

jbie by Associate II
  • 1518 Views
  • 1 replies
  • 0 kudos

Resolved! L6924D random status pin flicker in shutdown

Hello,i have a board with 10 L6924D on it, the schematic of each channel is derived from STEVAL-ISA076V1(*). Charging works as planned, CC/CV, correct max voltage and charge current and charge-end-current. Both status pins are connected to LEDs as on...

DoMl by Associate
  • 1454 Views
  • 1 replies
  • 0 kudos

Does ST plan to ever make another Eval6235 board?

I hope this is an appropriate group.  I don't see L6235Q anywhere. Is ST going to make any more Eval6235 boards?  There doesn't seem to be any on earth.  Choosing another controller is not an option. Mike

MikeSD by Associate
  • 1374 Views
  • 1 replies
  • 0 kudos

Resolved! What type of Diode

Hi, can anybody tell me what type of diode I see here?Marking is:GAAGP 843 Thanks.

Evaluation Board- EVSPIN32G4

I am buying a EVSPIN32G4 evaluation board. What are the things I should test or check on the new board for any faults or damages

Rajeswari by Associate III
  • 703 Views
  • 0 replies
  • 0 kudos

Resolved! Viper06 Buck mode converter, and AN4260

Hello, I need to be able to generate a small DC voltage from an AC voltage.  The App Note 4260 looked absolutely perfect - exactly what I needed - 12V 150mA buck converter.  Simple. no flyback transformers, etc.  But I was a bit confused as to the GN...

GGibb.1 by Associate II
  • 4571 Views
  • 3 replies
  • 1 kudos

Resolved! STUSB4710(A) doesn't output power

Dear Team, I recently created a custom PCB where I wanted to implement the STUSB4710(A) for charging a phone and other accessories. The STUSB4710 should be plug and play without the need of configuring the PDO because it is already selected. I based ...

MatthiasH_0-1710408850461.png MatthiasH_1-1710408899022.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.