Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SMPS Pulsing in hiccup mode

Hello, I have designed and assembled a SMPS based on the EVAL-STCH03-45W evaluation board. What I have noticed, is that the power supply is outputting 1 Hz pulses with short buzzing sounds. These symptoms usually mean the hiccup mode is activated. Ho...

smps.png
fing by Associate III
  • 1528 Views
  • 0 replies
  • 0 kudos

L4986 startup problems with external VCC supply

I am evaluating a PFC with the EVL4986-350W evaluation board.To be able to use Boost coils without the extra winding I want to supply the VCC voltage from a buck converter connected to the output voltage. The voltage from the buck is 17V.I have tried...

Jan-A by Associate
  • 795 Views
  • 0 replies
  • 0 kudos

PowerSTEP01 - is the ResetDevice command conditional?

I have a PowerSTEP01 that is behaving unexpectedly when I send the ResetDevice command.If I send it when my system starts then everything is ok when I check the STATUS register.However, if I send ResetDevice after the motor has been moved (sequence e...

CTapp.1 by Senior III
  • 636 Views
  • 0 replies
  • 0 kudos

SPV1050 with low volatge PV cell and Supercap

Dear allI use an STEVAL-ISV019V1 (Boost Mode) with a KXOB25-05X3F PV cell.When I connect a 330mF supercap to BATT, working at low light (200Lux) Store is being charged withing 30s. Not the SPV1050 tries to switch to the Supercap and restarts because ...

L293D

Hi everyone, I'm just starting in this field and I'm designing my first product. I'm designing a device that will use the L293D microchip and I'd like clarification on the following issues:1) There is a maximum value for the high voltage input curren...

Rafa by Associate
  • 1184 Views
  • 1 replies
  • 0 kudos

Disable L6924D maximum charging time

According to datasheet, L6924D has the possibility to set a maximum charging time, defined according to the capacitor connected in TPRG pin. But what should be done if the maximum charging time limit is undesirable? Can I short TPRG to GND to achieve...

MLuca.2 by Associate
  • 1609 Views
  • 2 replies
  • 0 kudos

Resolved! Need Help for PCB Design Problem Solution

Respected Sir/Ma'am,                                   I'm designing 2KW SMPS from reference schematics design of "STEVAL-ISA172V2: 2 KW fully digital AC-DC power supply (D-SMPS) evaluation board". I've not faced any obstacle in designing schematics ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.