Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

using stm32 firmware code to control vienna rectifer

I have used eDesignSuite to generate firmware code for my vienna rectifer. I need some more clarity/documentation on implementation of the code. Many things are unclear, such as at start-up, there is a pin dedicated to an relay, which will limit the ...

suyog800_0-1715663160038.png
suyog800 by Associate II
  • 786 Views
  • 0 replies
  • 0 kudos

PowerStep01 Current drop at medium speed

Hello,I have a problem to configure the powerstep01. The motor current drops at medium speeds.Current modestep clock mode1/16 microstep48 VoltI have set a low acceleration for testing. Everything is fine up to approx. 16 kHz (microstep). That's only ...

Barley_0-1715145622422.png
Barley by Associate II
  • 2463 Views
  • 5 replies
  • 0 kudos

What is the difference between LDL212 and LDL1117

I was picking a 5V high-performance LDO for RF mixer, and found that the parameters of LDL212 are very similar to those of the LDL1117 two series, the specific models are LDL212PU50R and LDL1117S50R, I checked their PSRR and output noise is almost th...

blackberryer_0-1715352458471.png blackberryer_1-1715352479274.png

Resolved! Need help identifying specific PMIC.

Dear Community,I'm a repair technician and I trying to identify a damaged component made by STMicroelectronics.Based on the surronding components and circuitry its a PMIC/DC-DC Coverter but I cannot find this specifc one.As you can see, all the infor...

PXL_20240508_101010963.jpg PXL_20240508_092815843-min.jpg

BTA16-800BW

Triac snubberless (bta-16-800bw) does not require a snubber in the circuit?Or would installing a snubber in the circuit have a good effect?The difference between BTA16-800BW and CW is the gate current difference.Will the current specification selecti...

Issue with ST1PS02 step-down converter

We are currently using the ST1PS02BQTR for powering a compact main board with BT connectivity (STM32WB5MMG), an IMU, and other ancillary blocks (LEDs, charge pump for LEDs, passives). The system is powered through two AAA batteries connected in serie...

como221e by Associate
  • 1425 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.