2024-05-02 6:56 PM
Dear all,
I am a BMS engineer looking for an automotive-grade BMS solution. Is L9961 good enough to develop an automotive-grade BMS for onboard battery pack monitoring? Do you have any other suggestions?
Thank you very much.
2024-05-09
5:49 AM
- last edited on
2024-05-14
7:27 AM
by
Lina_DABASINSKA
Dear @khwuuk ,
L9961 is not AEC-Q100 qualified. May I ask why you are looking for a 5-cell device?
What is the voltage range of your application?
I suggest you have a look at L9963E BMS IC, a 14 cells battery monitoring and protection chip for high-reliability automotive applications and energy storage systems.
L9963E is AEC-Q100 qualified, is Full ISO26262 compliant and ASIL-D systems ready.
Multiple L9963E can be connected in a daisy chain and communicates with the others by means of a vertical isolated interface L9963T.
Best Regards
2024-05-25 3:53 AM
Dear GS98,
Thank you very much for your information.
It seems that L9963E is a good solution. However, my application is for monitoring a single cell. We may not need the daisy chain function now, but an isolated interface is necessary. The voltage range is from 9V to 15V. Is L996E still a good solution?
Thank you very much.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.