2024-08-08 4:24 PM
Hello,
I am using the A5975 in an applicaiton that blows on power up. This sounds similar to the issue in the post below:
I have been unable to fix this with the exception of adding a resistor (10 Ohm or more) between the power supply and the A5975 (VBAT to VCC). This failure appears to happen only at power ON with a low impedance source. That is: power supply ON and plug in the power to target. I believe that connector bouncing makes this worse. Plugging or switching the power does not consistently cause a failure, but it does occur too frequently. If I plug in the power connector and apply power from the power supply, the voltage is ramped up over a few milliseconds. It never fails under this condition. I have yet to see this cause a failure, so it's likely a low impedance power supply switched on suddenly.
The schematic is essentially the same as the reference design in the datasheet.
Here's the schematic.
Any ideas what I am doing wrong here?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.