Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

A5975D Blow on Power Up

Hello, I am using the A5975 in an applicaiton that blows on power up. This sounds similar to the issue in the post below:https://community.st.com/t5/power-management/st1s41-step-down-switching-regulator-destroys-itself-on-low/m-p/171683 I have been u...

rmaier9_0-1723159208709.png
rmaier9 by Associate
  • 1030 Views
  • 0 replies
  • 0 kudos

Viper37HE

Good afternoon I'm designing a power supply and I have doubts about the transformer winding. I need to know the number of turns of the primary, secondary and auxiliary. Characteristics: Primary: 100-400VDC - 100kHZSecondary: 5V 4.8AAuxiliary: 12V 0.0...

STWBC2-HP UART Commands

Hi ST communityThe STWBC2-HP can be used with a GUI for configuration and plotting voltages and currents. The communication between GUI and firmware is done by UART. Is there any command list available that I can program my own interface on the compu...

Resolved! EP pin on L6924D

Hi! I'm using the L6924D chip for a university, and just saw a pin called EP. Searching on net, it is pointed that it's used for thermal purposes. Is that correct? If it is, what is the best approach for optimizing this parameter, considering the mod...

DRIVER LED STCMB1

Hello, I am having problems with the design of a 200W 36V LED driver.The LED driver works well up to 1A, I have tried to modify Rfmin and Rfmax to vary the frequency ranges but I cannot get it to work more than 1A.What is the solution to my problem?

AndresGG by Associate II
  • 778 Views
  • 0 replies
  • 0 kudos

Combining USB power via TCPP03 and external power source

I'm trying to combine an external +24V power source and the 5V USB power source into a single step-down converter to generate 3.3V.The USB power is managed by the TCPP03 chip for both providing and sourcing power. On my 24V line I have an eFuse TPS26...

tobiase by Associate
  • 670 Views
  • 0 replies
  • 0 kudos

STEVAL-HKI001V2 - board selection

Hello, I am an absolute beginner.  I am trying to create my first project to use with my STEVAL-HKI001V2 board. I cannot find this board in the list of boards to select from. How should I deal with the situation? Is there a way to add/import more boa...

adina25 by Associate II
  • 3095 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.