2019-05-01 11:33 AM
Hi,
there is a bug in newest STMB Cube with newest Firmware and STM32L151CCT.
Cube Version is 5.2.0, FreeRTOS V10.0.1.
I had a project with older Firmware which was imported from other project and I set the Memory usage to Static. I get an error in heap4.c that is may not come there ( for what heap when static operation). I'm usingf True Studion.
I find out that the Cube copies the file Middlewares/Third_Party/FreeRTOS/Source/portable/heap4.c to the project and this is not correct. I dont know hoe to hint Cube on generation this file. I have to delete it after each generation. I cannot regenerate it againg but I add the damaged file hier.
See attached for the project file. With this file you can produce i t at every generation.
Best regards,
Osto
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.