2025-12-10 3:41 AM - last edited on 2025-12-10 3:43 AM by Andrew Neil
Good morning.
Could anyone tell me about this error and how to resolve it.
C:/ST/STM32CubeIDE_1.19.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3 .rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: Oscillo_STM32G431CBU.elf section `.bss' will not fit in region `RAM'
C:/ST/STM32CubeIDE_1.19.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3 .rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: region `RAM' overflowed by 54928 bytes
I'm using IDE 1.19 to compile the code for a G431CBU
Grateful
Valter Matos
Solved! Go to Solution.
2025-12-10 11:51 AM - edited 2025-12-10 11:52 AM
I checked the .map
.bss.image_buffer
0x200000b4 0x12c00 ./Core/Src/ILI9488.ois 76.800 decimal, no way.
hth
KnarfB
2025-12-10 11:52 AM
@Andrew Neil wrote:@ValterMatos wrote:
/* Memories definition */
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 32K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 128K
}You've defined the 'RAM' region to be only 32K ?
That part only has 32K of ram.
2025-12-10 11:54 AM
@ValterMatos wrote:
/*
* sprites.c
*
* Created on: 3 maj 2024
* Author: Dominik
*/
#include "sprites.h"
#include "ILI9488.h"
const uint8_t trigRisingIcon[15][9] = {
{0 , 0 , 0 , 0 , WHITE , WHITE , WHITE , WHITE , WHITE},
{0 , 0 , 0 , 0 , WHITE , 0 , 0 , 0 , 0 },
{0 , 0 , 0 , 0 , WHITE , 0 , 0 , 0 , 0 },
{0 , 0 , 0 , 0 , WHITE , 0 , 0 , 0 , 0 },
{0 , 0 , 0 , 0 , WHITE , 0 , 0 , 0 , 0 },
{0 , 0 , 0 , 0 , WHITE , 0 , 0 , 0 , 0 },
{0 , 0 , 0 , WHITE , WHITE , WHITE , 0 , 0 , 0 },
{0 , 0 , WHITE , WHITE , WHITE , WHITE , WHITE , 0 , 0 },
{0 , WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , 0 },
{0 , 0 , 0 , 0 , WHITE , 0 , 0 , 0 , 0 },
{0 , 0 , 0 , 0 , WHITE , 0 , 0 , 0 , 0 },
{0 , 0 , 0 , 0 , WHITE , 0 , 0 , 0 , 0 },
{0 , 0 , 0 , 0 , WHITE , 0 , 0 , 0 , 0 },
{0 , 0 , 0 , 0 , WHITE , 0 , 0 , 0 , 0 },
{WHITE , WHITE , WHITE , WHITE , WHITE , 0 , 0 , 0 , 0 }
};
const uint8_t arrowUpDown[15][8] = {
{0 , 0 , 0 , WHITE , 0 , 0 , 0 , 0},
{0 , 0 , WHITE , WHITE , WHITE , 0 , 0 , 0},
{0 , WHITE , WHITE , WHITE , WHITE , WHITE , 0 , 0},
{WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , 0},
{0 , 0 , WHITE , WHITE , WHITE , 0 , 0 , 0},
{0 , 0 , WHITE , WHITE , WHITE , 0 , 0 , 0},
{0 , 0 , WHITE , WHITE , WHITE , 0 , 0 , 0},
{0 , 0 , WHITE , WHITE , WHITE , 0 , 0 , 0},
{0 , 0 , WHITE , WHITE , WHITE , 0 , 0 , 0},
{0 , 0 , WHITE , WHITE , WHITE , 0 , 0 , 0},
{0 , 0 , WHITE , WHITE , WHITE , 0 , 0 , 0},
{WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , 0},
{0 , WHITE , WHITE , WHITE , WHITE , WHITE , 0 , 0},
{0 , 0 , WHITE , WHITE , WHITE , 0 , 0 , 0},
{0 , 0 , 0 , WHITE , 0 , 0 , 0 , 0}
};
const uint8_t arrowLeftRight[7][15] = {
{0 , 0 , 0 , WHITE , 0 , 0 , 0 , 0 , 0 , 0 , 0 , WHITE , 0 , 0 , 0},
{0 , 0 , WHITE , WHITE , 0 , 0 , 0 , 0 , 0 , 0 , 0 , WHITE , WHITE , 0 , 0},
{0 , WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , 0},
{WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , WHITE},
{0 , WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , WHITE , 0},
{0 , 0 , WHITE , WHITE , 0 , 0 , 0 , 0 , 0 , 0 , 0 , WHITE , WHITE , 0 , 0},
{0 , 0 , 0 , WHITE , 0 , 0 , 0 , 0 , 0 , 0 , 0 , WHITE , 0 , 0 , 0}
};You've defined the tables as const, so no RAM is used for your tables. Check the .map file to see what is eating up your ram.
2025-12-10 11:58 AM
@KnarfB wrote:is 76.800 decimal,
So that's nearly the 50K overflow reported!
Presumably, this is allocating a full frame buffer in RAM?
2025-12-10 12:47 PM
The G431C has 128K flash and 32K RAM, and the CUBE MX is set in the configuration.
I still don't understand a 50K overflow.
I've already tried optimizing by reducing it by only 1K.
Maybe it's in the ILI9488 display buffer? I think it's unlikely.
I'll attach the codes for the ILI9488 display.
2025-12-10 12:49 PM
/*
* ILI9488.c
*
* Created on: Apr 29, 2021
* Author: hydra
*
* Modified by:
* Dominik Workshop, Eryk Możdżeń
* 8.04.2024
*
* Added image buffer
*/
#include "ILI9488.h"
#include "stdlib.h"
#include <stdbool.h>
#include <string.h>
extern SPI_HandleTypeDef hspi1;
extern DMA_HandleTypeDef hdma_spi1_tx;
extern uint8_t SPI1_TX_completed_flag;
/**
* @brief Buffer storing 4-bit color values for each LCD pixel.
* Each byte represents color information for two adjacent pixels, utilizing 4 bits per pixel
*/
static uint8_t image_buffer[ILI9488_TFTWIDTH*ILI9488_TFTHEIGHT/2 ] = {0};
/**
* @brief Macro to retrieve the color value of a pixel from the image buffer.
*
* @PAram x The x-coordinate of the pixel.
* @PAram y The y-coordinate of the pixel.
* @return The 4-bit color value of the specified pixel.
*/
#define IMG_BUFF_GET(x, y) (((x)%2)==0)?(image_buffer[((y)*240)+((x)/2)]>>4):(image_buffer[((y)*240)+((x)/2)]&0x0F)
/**
* @brief Macro to set the color value of a pixel in the image buffer.
*
* @PAram x The x-coordinate of the pixel.
* @PAram y The y-coordinate of the pixel.
* @PAram c The 4-bit color value to set for the pixel.
*/
#define IMG_BUF_SET(x, y, c) if(((x)%2)==0){image_buffer[((y)*(_width/2))+((x)/2)]&=0x0F;image_buffer[((y)*(_width/2))+((x)/2)]|=((c)<<4);} \
else{image_buffer[((y)*(_width/2))+((x)/2)]&=0xF0;image_buffer[((y)*(_width/2))+((x)/2)]|=(c);}
static uint8_t colors[16][3] = {
// r, g, b //
{0, 0, 0}, // black
{0x55, 0x55, 0x55}, // grey
{0xFF, 0xFF, 0xFF}, // white
{0, 0x55, 0}, // dark green
{0, 0xAA, 0}, // green
{0, 0xFF, 0}, // light green
{0, 0, 0xFF}, // dark blue
{0, 0x55, 0xFF}, // blue
{0, 0xAA, 0xFF}, // light blue
{0, 0xFF, 0xFF}, // cyan
{0xFF, 0, 0}, // red
{0xFF, 0x55, 0}, // light red
{0xFF, 0xAA, 0}, // orange
{0xFF, 0xFF, 0}, // yellow
{0xFF, 0, 0xFF}, // dark pink
{0xFF, 0x55, 0xFF} // pink
};
uint8_t tabcolor;
uint8_t mySPCR;
int16_t WIDTH;
int16_t HEIGHT;
int16_t _width;
int16_t _height;
int16_t cursor_x;
int16_t cursor_y;
uint16_t textcolor;
uint16_t textbgcolor;
uint8_t textsize_x;
uint8_t textsize_y;
uint8_t rotation;
void ILI9488_Init(void){
HAL_GPIO_WritePin(TFT_RST_GPIO_Port,TFT_RST_Pin, GPIO_PIN_RESET);
HAL_Delay(10);
HAL_GPIO_WritePin(TFT_RST_GPIO_Port,TFT_RST_Pin, GPIO_PIN_SET);
_width=ILI9488_TFTWIDTH;
_height=ILI9488_TFTHEIGHT;
writecommand(0xE0);
writedata(0x00);
writedata(0x03);
writedata(0x09);
writedata(0x08);
writedata(0x16);
writedata(0x0A);
writedata(0x3F);
writedata(0x78);
writedata(0x4C);
writedata(0x09);
writedata(0x0A);
writedata(0x08);
writedata(0x16);
writedata(0x1A);
writedata(0x0F);
writecommand(0XE1);
writedata(0x00);
writedata(0x16);
writedata(0x19);
writedata(0x03);
writedata(0x0F);
writedata(0x05);
writedata(0x32);
writedata(0x45);
writedata(0x46);
writedata(0x04);
writedata(0x0E);
writedata(0x0D);
writedata(0x35);
writedata(0x37);
writedata(0x0F);
writecommand(0XC0); //Power Control 1
writedata(0x17); //Vreg1out
writedata(0x15); //Verg2out
writecommand(0xC1); //Power Control 2
writedata(0x41); //VGH,VGL
writecommand(0xC5); //Power Control 3
writedata(0x00);
writedata(0x12); //Vcom
writedata(0x80);
writecommand(0x36); //Memory Access
writedata(0x48);
writecommand(0x36); // Interface Pixel Format
writedata(0x66); //18 bit
writecommand(0XB0); // Interface Mode Control
writedata(0x80); //SDO NOT USE
writecommand(0xB1); //Frame rate
writedata(0xA0); //60Hz
writecommand(0xB4); //Display Inversion Control
writedata(0x02); //2-dot
writecommand(0XB6); //Display Function Control RGB/MCU Interface Control
writedata(0x02); //MCU
writedata(0x02); //Source,Gate scan dieection
writecommand(0XE9); // Set Image Functio
writedata(0x00); // Disable 24 bit data
writecommand(0xF7); // Adjust Control
writedata(0xA9);
writedata(0x51);
writedata(0x2C);
writedata(0x82); // D7 stream, loose
writecommand(ILI9488_SLPOUT); //Exit Sleep
HAL_Delay(120);
writecommand(ILI9488_DISPON); //Display on
}
void setAddrWindow(uint16_t x0, uint16_t y0, uint16_t x1, uint16_t y1){
writecommand(ILI9488_CASET); // Column addr set
writedata(x0 >> 8);
writedata(x0 & 0xFF); // XSTART
writedata(x1 >> 8);
writedata(x1 & 0xFF); // XEND
writecommand(ILI9488_PASET); // Row addr set
writedata(y0 >> 8);
writedata(y0 & 0xff); // YSTART
writedata(y1 >> 8);
writedata(y1 & 0xff); // YEND
writecommand(ILI9488_RAMWR); // write to RAM
HAL_GPIO_WritePin(TFT_CS_GPIO_Port,TFT_CS_Pin, GPIO_PIN_RESET);
HAL_GPIO_WritePin(TFT_DC_GPIO_Port,TFT_DC_Pin, GPIO_PIN_SET);
}
void setScrollArea(uint16_t topFixedArea, uint16_t bottomFixedArea){
writecommand(0x33); // Vertical scroll definition
writedata(topFixedArea >> 8);
writedata(topFixedArea);
writedata((_height - topFixedArea - bottomFixedArea) >> 8);
writedata(_height - topFixedArea - bottomFixedArea);
writedata(bottomFixedArea >> 8);
writedata(bottomFixedArea);
}
void scroll(uint16_t pixels){
writecommand(0x37); // Vertical scrolling start address
writedata(pixels >> 8);
writedata(pixels);
}
/*
void pushColor(uint16_t color){
HAL_GPIO_WritePin(TFT_DC_GPIO_Port,TFT_DC_Pin,GPIO_PIN_SET);
HAL_GPIO_WritePin(TFT_CS_GPIO_Port,TFT_CS_Pin,GPIO_PIN_RESET);
write16BitColor(color);
HAL_GPIO_WritePin(TFT_CS_GPIO_Port,TFT_CS_Pin,GPIO_PIN_SET);
}
void pushColors(uint16_t *data, uint8_t len, uint8_t first){
uint16_t color;
uint8_t buff[len * 3 + 1];
uint16_t count = 0;
uint8_t lencount = len;
HAL_GPIO_WritePin(TFT_CS_GPIO_Port,TFT_CS_Pin,GPIO_PIN_RESET);
if (first == 1){
HAL_GPIO_WritePin(TFT_DC_GPIO_Port,TFT_DC_Pin,GPIO_PIN_SET);
}
while (lencount--){
color = *data++;
buff[count] = (((color & 0xF800) >> 11) * 255) / 31;
count++;
buff[count] = (((color & 0x07E0) >> 5) * 255) / 63;
count++;
buff[count] = ((color & 0x001F) * 255) / 31;
count++;
}
HAL_SPI_Transmit(&hspi1, buff, len * 3, 100);
HAL_GPIO_WritePin(TFT_CS_GPIO_Port,TFT_CS_Pin,GPIO_PIN_SET);
}
*/
/**
* @brief Draws image (img[h][w]) to a buffer
*
*/
void drawImageTransparent(uint16_t x, uint16_t y, uint16_t w, uint16_t h, const uint8_t* img){
if ((x >= _width) || (y >= _height))
return;
if ((x + w - 1) >= _width)
w = _width - x;
if ((y + h - 1) >= _height)
h = _height - y;
for (uint16_t i = 0; i < h; i++) {
for (uint16_t o = 0; o < w; o++) {
if (img[i * w + o] != BLACK) {
drawPixel(x + o, y + i, img[i * w + o]);
}
}
}
}
/**
* @brief Draws image (img[h][w]) to a buffer with every non black pixel colored to given color
*
*/
void drawImageTransparentColored(uint16_t x, uint16_t y, uint16_t w, uint16_t h, const uint8_t* img, uint8_t color){
if ((x >= _width) || (y >= _height))
return;
if ((x + w - 1) >= _width)
w = _width - x;
if ((y + h - 1) >= _height)
h = _height - y;
for (uint16_t i = 0; i < h; i++) {
for (uint16_t o = 0; o < w; o++) {
if (img[i * w + o] != BLACK) {
drawPixel(x + o, y + i, color);
}
}
}
}
/**
* @brief Draws image (img[h][w]) to a buffer
*
*/
void drawImage(const uint8_t* img, uint16_t x, uint16_t y, uint16_t w, uint16_t h){
if ((x >= _width) || (y >= _height))
return;
if ((x + w - 1) >= _width)
w = _width - x;
if ((y + h - 1) >= _height)
h = _height - y;
for (uint16_t i = 0; i < h; i++) {
for (uint16_t o = 0; o < w; o++) {
drawPixel(x + o, y + i, img[i * w + o]);
}
}
}
/**
* @brief Fills the entire screen with the specified color.
*
* @PAram color The 4-bit color value to fill the screen with.
*/
void fillScreen(uint8_t color){
fillRect(0, 0, _width, _height, color);
}
/**
* @brief Sets all pixels to black
*/
void clearScreen(){
memset(image_buffer, BLACK, sizeof(image_buffer));
}
/**
* @brief Sets the pixel at the specified location to the specified color.
*
*
* @PAram x The x-coordinate of the pixel.
* @PAram y The y-coordinate of the pixel.
* @PAram color The color value to set for the pixel.
*/
void drawPixel(int16_t x, int16_t y, uint8_t color){
if ((x < 0) || (x >= _width) || (y < 0) || (y >= _height))
return;
IMG_BUF_SET(x, y, color);
}
void drawFastVLine(int16_t x, int16_t y, int16_t h, uint16_t color){
if ((x >= _width) || (y >= _height))
return;
if ((y + h - 1) >= _height)
h = _height - y;
for(uint16_t i = 0; i < h; ++i){
IMG_BUF_SET(x, y+i, color);
}
}
void drawFastVDottedLine(int16_t x, int16_t y, int16_t h, uint16_t color){
if ((x >= _width) || (y >= _height))
return;
if ((y + h - 1) >= _height)
h = _height - y;
for(uint16_t i = 0; i < h; i+=2){
IMG_BUF_SET(x, y+i, color);
}
}
void drawFastHLine(int16_t x, int16_t y, int16_t w, uint16_t color){
if ((x >= _width) || (y >= _height))
return;
if ((x + w - 1) >= _width)
w = _width - x;
for(uint16_t i = 0; i < w; ++i){
IMG_BUF_SET(x+i, y, color);
}
}
void drawFastHDottedLine(int16_t x, int16_t y, int16_t w, uint16_t color){
if ((x >= _width) || (y >= _height))
return;
if ((x + w - 1) >= _width)
w = _width - x;
for(uint16_t i = 0; i < w; i+=2){
IMG_BUF_SET(x+i, y, color);
}
}
void drawLine(int16_t x0, int16_t y0, int16_t x1, int16_t y1,uint16_t color){
if (x0 == x1) {
if (y0 > y1)
_swap_int16_t(y0, y1);
drawFastVLine(x0, y0, y1 - y0 + 1, color);
} else if (y0 == y1) {
if (x0 > x1)
_swap_int16_t(x0, x1);
drawFastHLine(x0, y0, x1 - x0 + 1, color);
} else {
writeLine(x0, y0, x1, y1, color);
}
}
void writeLine(int16_t x0, int16_t y0, int16_t x1, int16_t y1,uint16_t color){
int16_t steep = abs(y1 - y0) > abs(x1 - x0);
if (steep) {
_swap_int16_t(x0, y0);
_swap_int16_t(x1, y1);
}
if (x0 > x1) {
_swap_int16_t(x0, x1);
_swap_int16_t(y0, y1);
}
int16_t dx, dy;
dx = x1 - x0;
dy = abs(y1 - y0);
int16_t err = dx / 2;
int16_t ystep;
if (y0 < y1) {
ystep = 1;
} else {
ystep = -1;
}
for (; x0 <= x1; x0++) {
if (steep) {
IMG_BUF_SET(y0, x0, color)
} else {
IMG_BUF_SET(x0, y0, color)
}
err -= dy;
if (err < 0) {
y0 += ystep;
err += dx;
}
}
}
void fillRect(int16_t x, int16_t y, int16_t w, int16_t h, uint8_t color){
if ((x >= _width) || (y >= _height))
return;
if ((x + w - 1) >= _width)
w = _width - x;
if ((y + h - 1) >= _height)
h = _height - y;
for(int16_t i = 0; i < w; ++i){
for(int16_t j = 0; j < h; ++j){
IMG_BUF_SET(x+i, y+j, color);
}
}
}
void setRotation(uint8_t r){
writecommand(ILI9488_MADCTL);
rotation = r % 4; // can't be higher than 3
switch (rotation) {
case 0:
writedata(MADCTL_MX | MADCTL_BGR);
_width = ILI9488_TFTWIDTH;
_height = ILI9488_TFTHEIGHT;
break;
case 1:
writedata(MADCTL_MV | MADCTL_BGR);
_width = ILI9488_TFTHEIGHT;
_height = ILI9488_TFTWIDTH;
break;
case 2:
writedata(MADCTL_MY | MADCTL_BGR);
_width = ILI9488_TFTWIDTH;
_height = ILI9488_TFTHEIGHT;
break;
case 3:
writedata(MADCTL_MX | MADCTL_MY | MADCTL_MV | MADCTL_BGR);
_width = ILI9488_TFTHEIGHT;
_height = ILI9488_TFTWIDTH;
break;
}
}
void invertDisplay(uint8_t i){
writecommand(i ? ILI9488_INVON : ILI9488_INVOFF);
}
uint16_t color565(uint8_t r, uint8_t g, uint8_t b){
return ((r & 0xF8) << 8) | ((g & 0xFC) << 3) | (b >> 3);
}
void spiwrite(uint8_t data){
HAL_SPI_Transmit(&hspi1, &data, 1, 1);
}
void writecommand(uint8_t c){
HAL_GPIO_WritePin(TFT_DC_GPIO_Port,TFT_DC_Pin,GPIO_PIN_RESET);
HAL_GPIO_WritePin(TFT_CS_GPIO_Port,TFT_CS_Pin,GPIO_PIN_RESET);
HAL_SPI_Transmit(&hspi1, &c, 1, 1);
HAL_GPIO_WritePin(TFT_CS_GPIO_Port,TFT_CS_Pin,GPIO_PIN_SET);
}
void write16BitColor(uint16_t color){
uint8_t r = (color & 0xF800) >> 11;
uint8_t g = (color & 0x07E0) >> 5;
uint8_t b = color & 0x001F;
r = (r * 255) / 31;
g = (g * 255) / 63;
b = (b * 255) / 31;
HAL_SPI_Transmit(&hspi1, &r, 1, 1);
HAL_SPI_Transmit(&hspi1, &g, 1, 1);
HAL_SPI_Transmit(&hspi1, &b, 1, 1);
}
void writedata(uint8_t d){
HAL_GPIO_WritePin(TFT_DC_GPIO_Port,TFT_DC_Pin,GPIO_PIN_SET);
HAL_GPIO_WritePin(TFT_CS_GPIO_Port,TFT_CS_Pin,GPIO_PIN_RESET);
HAL_SPI_Transmit(&hspi1, &d, 1, 1);
HAL_GPIO_WritePin(TFT_CS_GPIO_Port,TFT_CS_Pin,GPIO_PIN_SET);
}
void testLines(uint8_t color){
//unsigned long start, t;
int x1, y1, x2, y2, w = _width, h = _height;
fillScreen(BLACK);
x1 = y1 = 0;
y2 = h - 1;
for (x2 = 0; x2 < w; x2 += 6)
drawLine(x1, y1, x2, y2, color);
x2 = w - 1;
for (y2 = 0; y2 < h; y2 += 6)
drawLine(x1, y1, x2, y2, color);
fillScreen(BLACK);
x1 = w - 1;
y1 = 0;
y2 = h - 1;
for (x2 = 0; x2 < w; x2 += 6)
drawLine(x1, y1, x2, y2, color);
x2 = 0;
for (y2 = 0; y2 < h; y2 += 6)
drawLine(x1, y1, x2, y2, color);
fillScreen(BLACK);
x1 = 0;
y1 = h - 1;
y2 = 0;
for (x2 = 0; x2 < w; x2 += 6)
drawLine(x1, y1, x2, y2, color);
x2 = w - 1;
for (y2 = 0; y2 < h; y2 += 6)
drawLine(x1, y1, x2, y2, color);
fillScreen(ILI9488_BLACK);
x1 = w - 1;
y1 = h - 1;
y2 = 0;
for (x2 = 0; x2 < w; x2 += 6)
drawLine(x1, y1, x2, y2, color);
x2 = 0;
for (y2 = 0; y2 < h; y2 += 6)
drawLine(x1, y1, x2, y2, color);
}
void sendasIO(uint8_t d){
for (uint8_t bit = 0x80; bit; bit >>= 1) {
if (d & bit) {
//_mosi->setHigh();
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_7, GPIO_PIN_SET);
} else {
//_mosi->setLow();
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_7, GPIO_PIN_RESET);
}
//_sck->setHigh();
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_SET);
//HAL_Delay(4);
//__ASM volatile ("NOP");
//_sck->setLow();
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_RESET);
}
}
/*void ILI9488::commandList(uint8_t *addr)
{
uint8_t numCommands, numArgs;
uint16_t ms;
numCommands = pgm_read_byte(addr++);
while (numCommands--) {
writecommand(pgm_read_byte(addr++));
numArgs = pgm_read_byte(addr++);
ms = numArgs & 0x80;
numArgs &= ~0x80;
while (numArgs--) {
writedata(pgm_read_byte(addr++));
}
if (ms) {
ms = pgm_read_byte(addr++); // Read post-command delay time (ms)
if (ms == 255)
ms = 500; // If 255, delay for 500 ms
delay(ms);
}
}
}*/
void ILI9341_Draw_Colour(uint16_t Colour){
//SENDS COLOUR
uint8_t r = (Colour & 0xF800) >> 11;
uint8_t g = (Colour & 0x07E0) >> 5;
uint8_t b = Colour & 0x001F;
r = (r * 255) / 31;
g = (g * 255) / 63;
b = (b * 255) / 31;
unsigned char TempBuffer[3] = { r, g ,b };
for (uint32_t j = 0; j < 480*320; j++){
HAL_GPIO_WritePin(TFT_DC_GPIO_Port, TFT_DC_Pin, GPIO_PIN_SET);
HAL_GPIO_WritePin(TFT_CS_GPIO_Port, TFT_CS_Pin, GPIO_PIN_RESET);
SPI1_TX_completed_flag = 0;
HAL_SPI_Transmit_DMA(&hspi1, TempBuffer, 3);
while (SPI1_TX_completed_flag == 0)
HAL_GPIO_WritePin(TFT_CS_GPIO_Port, TFT_CS_Pin, GPIO_PIN_SET);
}
}
//INTERNAL FUNCTION OF LIBRARY
/*Sends block colour information to LCD*/
void ILI9341_Draw_Colour_Burst(uint16_t Colour, uint32_t Size){
//SENDS COLOUR
uint32_t Buffer_Size = 0;
if ((Size * 2) < BURST_MAX_SIZE){
Buffer_Size = Size;
}
else{
Buffer_Size = BURST_MAX_SIZE;
}
HAL_GPIO_WritePin(TFT_DC_GPIO_Port, TFT_DC_Pin, GPIO_PIN_SET);
HAL_GPIO_WritePin(TFT_CS_GPIO_Port, TFT_CS_Pin, GPIO_PIN_RESET);
// unsigned char MSB_color = Colour >> 8;
uint8_t r = (Colour & 0xF800) >> 11;
uint8_t g = (Colour & 0x07E0) >> 5;
uint8_t b = Colour & 0x001F;
r = (r * 255) / 31;
g = (g * 255) / 63;
b = (b * 255) / 31;
unsigned char burst_buffer[Buffer_Size];
for (uint32_t j = 0; j < Buffer_Size; j += 3){
burst_buffer[j] = r;
burst_buffer[j + 1] = g;
burst_buffer[j + 2] = b;
}
uint32_t Sending_Size = Size * 3;
uint32_t Sending_in_Block = Sending_Size / Buffer_Size;
uint32_t Remainder_from_block = Sending_Size % Buffer_Size;
if (Sending_in_Block != 0){
for (uint32_t j = 0; j < (Sending_in_Block); j++){
SPI1_TX_completed_flag = 0;
HAL_SPI_Transmit_DMA(&hspi1, (unsigned char*) burst_buffer, Buffer_Size);
while (SPI1_TX_completed_flag == 0);
}
}
//REMAINDER!
if (Remainder_from_block > 0)
{
SPI1_TX_completed_flag = 0;
HAL_SPI_Transmit_DMA(&hspi1, (unsigned char*) burst_buffer, Remainder_from_block);
while (SPI1_TX_completed_flag == 0);
}
HAL_GPIO_WritePin(TFT_CS_GPIO_Port, TFT_CS_Pin, GPIO_PIN_SET);
}
//FILL THE ENTIRE SCREEN WITH SELECTED COLOUR (either #define-d ones or custom 16bit)
/*Sets address (entire screen) and Sends Height*Width ammount of colour information to LCD*/
void ILI9341_Fill_Screen(uint16_t Colour){
// LCD_Address_Set(xsta,ysta+OFFSET_Y,xend-1,yend-1+OFFSET_Y);/
setAddrWindow(0, 0, ILI9488_TFTHEIGHT-1, ILI9488_TFTWIDTH-1);
ILI9341_Draw_Colour_Burst(Colour, ILI9488_TFTWIDTH * ILI9488_TFTHEIGHT);
}
void ILI9341_Fill_Screen1(uint16_t x, uint16_t y, uint16_t w, uint16_t h,uint16_t Colour){
// LCD_Address_Set(xsta,ysta+OFFSET_Y,xend-1,yend-1+OFFSET_Y);/
setAddrWindow(x, y, h-1, w-1);
ILI9341_Draw_Colour_Burst(Colour, w * h);
}
//static void WriteDataDMA(const void *data, uint16_t length)
//{
// txComplete = false;
// HAL_SPI_Transmit_DMA(&hspi1, (uint8_t *)data, length);
//}
//
//static void WaitForDMAWriteComplete(void)
//{
// while (txComplete == false)
// {
// }
//}
//
//void ILI9341FilledRectangle(uint16_t x, uint16_t y, uint16_t width, uint16_t height, colour_t colour)
//{
// colour_t dmaBuffer[DMA_BUFFER_SIZE];
// uint8_t i;
// uint32_t totalBytesToWrite;
// uint32_t bytesToWriteThisTime;
//
// for (i = 0U; i < DMA_BUFFER_SIZE; i++)
// {
// dmaBuffer[i] = __builtin_bswap16(colour);
// }
//
// setAddrWindow(x, y, x + ILI9488_TFTWIDTH - 1U, y + ILI9488_TFTHEIGHT - 1U);
// totalBytesToWrite = (uint32_t)width * (uint32_t)height * (uint32_t)sizeof(colour_t);
// bytesToWriteThisTime = DMA_BUFFER_SIZE * (uint16_t)sizeof(colour_t);
//
// while (totalBytesToWrite > 0UL)
// {
// if (totalBytesToWrite < bytesToWriteThisTime)
// {
// bytesToWriteThisTime = totalBytesToWrite;
// }
// totalBytesToWrite -= bytesToWriteThisTime;
//
// WriteDataDMA(&dmaBuffer, bytesToWriteThisTime);
// WaitForDMAWriteComplete();
// }
//}
//
//static void filledRectangleClip(int16_t x, int16_t y, uint16_t width, uint16_t height, colour_t colour)
//{
// int16_t x_end;
// int16_t y_end;
//
// if (x > (int16_t)ILI9488_TFTWIDTH - 1 || y > (int16_t)ILI9488_TFTHEIGHT - 1)
// {
// return;
// }
//
// if (x + (int16_t)width < 0 || y + (int16_t)height < 0)
// {
// return;
// }
//
// if (x < 0)
// {
// width -= (uint16_t)-x;
// x = 0;
// }
//
// if (y < 0)
// {
// height -= (uint16_t)-y;
// y = 0;
// }
//
// x_end = x + (int16_t)width - 1;
// if (x_end >(int16_t)ILI9488_TFTWIDTH - 1)
// {
// x_end = (int16_t)ILI9488_TFTWIDTH - 1;
// }
//
// y_end = y + (int16_t)height - 1;
// if (y_end > (int16_t)ILI9488_TFTHEIGHT - 1)
// {
// y_end = (int16_t)ILI9488_TFTHEIGHT - 1;
// }
//
// // clipped sizes
// width = (uint16_t)(x_end - x + 1);
// height = (uint16_t)(y_end - y + 1);
//
// ILI9341FilledRectangle((uint16_t)x, (uint16_t)y, width, height, colour);
//}
//
//
//void GraphicsClear(colour_t colour)
//{
// filledRectangleClip(0U, 0U, (uint16_t)ILI9488_TFTWIDTH, (uint16_t)ILI9488_TFTHEIGHT, colour);
//}
//
void LCD_Char(int16_t x, int16_t y, const GFXglyph *glyph, const GFXfont *font, uint8_t size, uint32_t color24){
uint8_t *bitmap = font -> bitmap;
uint16_t bo = glyph -> bitmapOffset;
uint8_t bits = 0, bit = 0;
uint16_t set_pixels = 0;
uint8_t cur_x, cur_y;
for (cur_y = 0; cur_y < glyph -> height; cur_y++){
for (cur_x = 0; cur_x < glyph -> width; cur_x++){
if (bit == 0){
bits = (*(const unsigned char *)(&bitmap[bo++]));
bit = 0x80;
}
if (bits & bit) set_pixels++;
else if (set_pixels > 0){
fillRect(x + (glyph -> xOffset + cur_x - set_pixels) * size, y + (glyph -> yOffset + cur_y) * size, size * set_pixels, size, color24);
set_pixels = 0;
}
bit >>= 1;
}
if (set_pixels > 0){
fillRect(x + (glyph -> xOffset + cur_x-set_pixels) * size, y + (glyph -> yOffset + cur_y) * size, size * set_pixels, size, color24);
set_pixels = 0;
}
}
}
void LCD_Font(uint16_t x, uint16_t y, const char *text, const GFXfont *p_font, uint8_t size, uint32_t color24){
int16_t cursor_x = x;
int16_t cursor_y = y;
GFXfont font;
memcpy(&font, p_font, sizeof(GFXfont));
for (uint16_t text_pos = 0; text_pos < strlen(text); text_pos++){
char c = text[text_pos];
if (c == '\n'){
cursor_x = x;
cursor_y += font.yAdvance * size;
}
else if (c >= font.first && c <= font.last && c != '\r'){
GFXglyph glyph;
memcpy(&glyph, &font.glyph[c - font.first], sizeof(GFXglyph));
LCD_Char(cursor_x, cursor_y, &glyph, &font, size, color24);
cursor_x += glyph.xAdvance * size;
}
}
}
void drawImage2(){
}
void drawCanva(){
int x =0;
int y=20;
int w = _width;
int h = _height;
if ((x >= _width) || (y >= _height))
return;
if ((x + w - 1) >= _width)
w = _width - x;
if ((y + h - 1) >= _height)
h = _height - y;
setAddrWindow(x, y, x + w - 1, y + h - 1);
HAL_GPIO_WritePin(TFT_DC_GPIO_Port,TFT_DC_Pin,GPIO_PIN_SET);
HAL_GPIO_WritePin(TFT_CS_GPIO_Port,TFT_CS_Pin,GPIO_PIN_RESET);
uint8_t linebuff[w * 3 + 1];
uint16_t color;
for (uint16_t i = 0; i < h; i++) {
uint16_t pixcount = 0;
for (uint16_t o = 0; o < w; o++) {
// Check if it's a horizontal grid line
if ((i % 60 == 0) || (i == 319- y)) {
color = ILI9488_DARKGREY; // White
} else {
// Check if it's a vertical grid line
if ((o % 60 == 0) || (o == 479)) {
color = ILI9488_DARKGREY; // White
} else {
color = 0x0000; // Black
}
}
linebuff[pixcount] = (((color & 0xF800) >> 11) * 255)
/ 31;
pixcount++;
linebuff[pixcount] = (((color & 0x07E0) >> 5) * 255)
/ 63;
pixcount++;
linebuff[pixcount] = ((color & 0x001F) * 255) / 31;
pixcount++;
}
HAL_SPI_Transmit(&hspi1, linebuff, w * 3, 100);
}
HAL_GPIO_WritePin(TFT_CS_GPIO_Port,TFT_CS_Pin,GPIO_PIN_SET);
}
/**
* @brief Renders an image stored in an image buffer to the LCD screen
*
*/
void imageRender(){
setAddrWindow(0, 0, _width - 1, _height - 1);
HAL_GPIO_WritePin(TFT_DC_GPIO_Port,TFT_DC_Pin,GPIO_PIN_SET);
HAL_GPIO_WritePin(TFT_CS_GPIO_Port,TFT_CS_Pin,GPIO_PIN_RESET);
// Buffer to hold pixel color data for a single line of the screen
uint8_t linebuff[_width * 3 + 1];
// Iterate through each row (height) of the screen
for (uint16_t h = 0; h < _height; h++){
// Iterate through each column (width) of the screen
for (uint16_t w = 0; w < _width; w++){
// Retrieve the pixel color index from the image buffer
uint8_t pixel_color = IMG_BUFF_GET(w, h);
// Retrieve the RGB color values corresponding to the pixel color index
linebuff[3*w + 0] = colors[pixel_color][0]; // r
linebuff[3*w + 1] = colors[pixel_color][1]; // g
linebuff[3*w + 2] = colors[pixel_color][2]; // b
}
HAL_SPI_Transmit(&hspi1, linebuff, _width * 3, 100);
}
HAL_GPIO_WritePin(TFT_CS_GPIO_Port,TFT_CS_Pin,GPIO_PIN_SET);
}
void drawRectangleRoundedFrame(int16_t x, int16_t y, int16_t w, int16_t h, uint8_t color) {
drawFastHLine(x + 5, y, w - 9, color); // Top line
drawFastHLine(x + 5, y + h, w - 9, color); // Bottom line
drawFastVLine(x, y + 5, h - 9, color); // Left line
drawFastVLine(x + w, y + 5, h - 9, color); // Right line
// right top corner
drawFastHLine(x + 3, y + 1, 2, color); // Top line
drawFastVLine(x + 1, y + 3, 2, color); // Left line
drawPixel(x + 2, y + 2, color);
// left top corner
drawFastHLine(x - 4 + w, y + 1, 2, color); // Top line
drawFastVLine(x - 1 + w, y + 3, 2, color); // Right line
drawPixel(x - 2 + w, y + 2, color);
// right bottom corner
drawFastHLine(x + 3, y - 1 + h, 2, color); // Bottom line
drawFastVLine(x + 1, y - 4 + h, 2, color); // Left line
drawPixel(x + 2, y - 2 + h, color);
// left bottom corner
drawFastHLine(x - 4 + w, y - 1 + h, 2, color); // Bottom line
drawFastVLine(x - 1 + w, y - 4 + h, 2, color); // Left line
drawPixel(x - 2 + w, y - 2 + h, color);
}
2025-12-10 12:50 PM
/*
* ILI9488.h
*
* Created on: Apr 29, 2021
* Author: hydra
*
* Modified by:
* Dominik Workshop, Eryk Możdżeń
* 8.04.2024
*
* Added image buffer
*/
#ifndef ILI9488_H_
#define ILI9488_H_
#include <math.h>
#include "main.h"
enum colors{
BLACK,
GREY,
WHITE,
DARK_GREEN,
GREEN,
LIGHT_GREEN,
DARK_BLUE,
BLUE,
LIGHT_BLUE,
CYAN,
RED,
LIGHT_RED,
ORANGE,
YELLOW,
DARK_PINK,
PINK
};
#define DMA_BUFFER_SIZE 64U
#define BURST_MAX_SIZE 750
#define ILI9488_TFTWIDTH 320
#define ILI9488_TFTHEIGHT 480
#define ILI9488_NOP 0x00
#define ILI9488_SWRESET 0x01
#define ILI9488_RDDID 0x04
#define ILI9488_RDDST 0x09
#define ILI9488_SLPIN 0x10
#define ILI9488_SLPOUT 0x11
#define ILI9488_PTLON 0x12
#define ILI9488_NORON 0x13
#define ILI9488_RDMODE 0x0A
#define ILI9488_RDMADCTL 0x0B
#define ILI9488_RDPIXFMT 0x0C
#define ILI9488_RDIMGFMT 0x0D
#define ILI9488_RDSELFDIAG 0x0F
#define ILI9488_INVOFF 0x20
#define ILI9488_INVON 0x21
#define ILI9488_GAMMASET 0x26
#define ILI9488_DISPOFF 0x28
#define ILI9488_DISPON 0x29
#define ILI9488_CASET 0x2A
#define ILI9488_PASET 0x2B
#define ILI9488_RAMWR 0x2C
#define ILI9488_RAMRD 0x2E
#define ILI9488_PTLAR 0x30
#define ILI9488_MADCTL 0x36
#define ILI9488_PIXFMT 0x3A
#define ILI9488_FRMCTR1 0xB1
#define ILI9488_FRMCTR2 0xB2
#define ILI9488_FRMCTR3 0xB3
#define ILI9488_INVCTR 0xB4
#define ILI9488_DFUNCTR 0xB6
#define ILI9488_PWCTR1 0xC0
#define ILI9488_PWCTR2 0xC1
#define ILI9488_PWCTR3 0xC2
#define ILI9488_PWCTR4 0xC3
#define ILI9488_PWCTR5 0xC4
#define ILI9488_VMCTR1 0xC5
#define ILI9488_VMCTR2 0xC7
#define ILI9488_RDID1 0xDA
#define ILI9488_RDID2 0xDB
#define ILI9488_RDID3 0xDC
#define ILI9488_RDID4 0xDD
#define ILI9488_GMCTRP1 0xE0
#define ILI9488_GMCTRN1 0xE1
//#define ILI9488_PWCTR6 0xFC
// Color definitions
#define ILI9488_BLACK 0x0000 /* 0, 0, 0 */
#define ILI9488_NAVY 0x000F /* 0, 0, 128 */
#define ILI9488_DARKGREEN 0x03E0 /* 0, 128, 0 */
#define ILI9488_DARKCYAN 0x03EF /* 0, 128, 128 */
#define ILI9488_MAROON 0x7800 /* 128, 0, 0 */
#define ILI9488_PURPLE 0x780F /* 128, 0, 128 */
#define ILI9488_OLIVE 0x7BE0 /* 128, 128, 0 */
#define ILI9488_LIGHTGREY 0xC618 /* 192, 192, 192 */
#define ILI9488_DARKGREY 0x7BEF /* 128, 128, 128 */
#define ILI9488_BLUE 0x001F /* 0, 0, 255 */
#define ILI9488_GREEN 0x07E0 /* 0, 255, 0 */
#define ILI9488_CYAN 0x07FF /* 0, 255, 255 */
#define ILI9488_RED 0xF800 /* 255, 0, 0 */
#define ILI9488_MAGENTA 0xF81F /* 255, 0, 255 */
#define ILI9488_YELLOW 0xFFE0 /* 255, 255, 0 */
#define ILI9488_WHITE 0xFFFF /* 255, 255, 255 */
#define ILI9488_ORANGE 0xFD20 /* 255, 165, 0 */
#define ILI9488_GREENYELLOW 0xAFE5 /* 173, 255, 47 */
#define ILI9488_PINK 0xF81F
typedef uint16_t colour_t;
#define MADCTL_MY 0x80
#define MADCTL_MX 0x40
#define MADCTL_MV 0x20
#define MADCTL_ML 0x10
#define MADCTL_RGB 0x00
#define MADCTL_BGR 0x08
#define MADCTL_MH 0x04
#define _swap_int16_t(a, b) \
{int16_t t = a; \
a = b; \
b = t; \
}
typedef struct { // Data stored PER GLYPH
uint16_t bitmapOffset; // Pointer into GFXfont->bitmap
uint8_t width, height; // Bitmap dimensions in pixels
uint8_t xAdvance; // Distance to advance cursor (x axis)
int8_t xOffset, yOffset; // Dist from cursor position to UL corner
} GFXglyph;
typedef struct { // Data stored for FONT AS A WHOLE:
uint8_t *bitmap; // Glyph bitmaps, concatenated
GFXglyph *glyph; // Glyph array
uint8_t first, last; // ASCII extents
uint8_t yAdvance; // Newline distance (y axis)
} GFXfont;
/* GENERAL CONFIGURATIONS */
#define _DEGUG_MODE 1
#define SINGLE_IO_MODE 1
void ILI9488_Init(void);
void begin(void);
void setAddrWindow(uint16_t x0, uint16_t y0, uint16_t x1, uint16_t y1);
void setScrollArea(uint16_t topFixedArea, uint16_t bottomFixedArea);
void scroll(uint16_t pixels);
void pushColor(uint16_t color);
void pushColors(uint16_t *data, uint8_t len, uint8_t first);
void drawImageTransparent(uint16_t x, uint16_t y, uint16_t w, uint16_t h, const uint8_t* img);
void drawImageTransparentColored(uint16_t x, uint16_t y, uint16_t w, uint16_t h, const uint8_t* img, uint8_t color);
void drawImage(const uint8_t* img, uint16_t x, uint16_t y, uint16_t w, uint16_t h);
void fillScreen(uint8_t color);
void drawPixel(int16_t x, int16_t y, uint8_t color);
void drawFastVLine(int16_t x, int16_t y, int16_t h, uint16_t color);
void drawFastVDottedLine(int16_t x, int16_t y, int16_t h, uint16_t color);
void drawFastHLine(int16_t x, int16_t y, int16_t w, uint16_t color);
void drawFastHDottedLine(int16_t x, int16_t y, int16_t w, uint16_t color);
void drawLine(int16_t x0, int16_t y0, int16_t x1, int16_t y1,uint16_t color);
void writeLine(int16_t x0, int16_t y0, int16_t x1, int16_t y1,uint16_t color);
void fillRect(int16_t x, int16_t y, int16_t w, int16_t h, uint8_t color);
void setRotation(uint8_t r);
void invertDisplay(uint8_t i);
uint16_t color565(uint8_t r, uint8_t g, uint8_t b);
void spiwrite(uint8_t data);
void writecommand(uint8_t c);
void write16BitColor(uint16_t color);
void writedata(uint8_t d);
void testLines(uint8_t color);
void sendasIO(uint8_t d);
void ILI9341FilledRectangle(uint16_t x, uint16_t y, uint16_t width, uint16_t height, colour_t colour);
void GraphicsClear(colour_t colour);
void ILI9341_Fill_Screen(uint16_t Colour);
void ILI9341_Draw_Colour(uint16_t Colour);
void ILI9341_Fill_Screen1(uint16_t x, uint16_t y, uint16_t w, uint16_t h,uint16_t Colour);
void LCD_Font(uint16_t x, uint16_t y, const char *text, const GFXfont *p_font, uint8_t size, uint32_t color24);
void drawCanva();
void imageRender();
void clearScreen();
void drawRectangleRoundedFrame(int16_t x, int16_t y, int16_t w, int16_t h, uint8_t color);
#endif /* ILI9488_H_ */
2025-12-10 12:52 PM
I've also attached the .map file, which I didn't quite understand.
2025-12-10 12:57 PM
The ".map" file is too large to attach.
2025-12-10 1:07 PM - edited 2025-12-10 1:10 PM
So you have:
#define ILI9488_TFTWIDTH 320
#define ILI9488_TFTHEIGHT 480and
/**
* @brief Buffer storing 4-bit color values for each LCD pixel.
* Each byte represents color information for two adjacent pixels, utilizing 4 bits per pixel
*/
static uint8_t image_buffer[ ILI9488_TFTWIDTH*ILI9488_TFTHEIGHT/2 ] = {0};which becomes
static uint8_t image_buffer[ 320*480/2 ] = {0};320*480/2 = 76800 bytes !
ie, 75K bytes
Which is exactly what @KnarfB said earlier - from the map file.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.