2021-08-10 5:26 AM
Hi, I am trying to build a Simulink model by using the STM32 Embedded Target. By following the instructions provided in the manual, I added the path in Matlab, and, in Simulink, I went to " Configuration Parameters --> Code Generation " and selected the "System target file" stm32.tlc from the list. However, I get several warnings/errors.
1 ) Warning: An error occurred while evaluating "loc_register_device" in
"C:\MATLAB\STM32-MAT\STM32\script\sl_customization.p": Support for the RTW.HWDeviceRegistry class has been removed.
2) Warning: Error executing the PostApplyCallback of the target "stm32.tlc":
Path not found ===> STM32CubeMx not installed or modify "STM32CubeMx installation path"
field.
The sl_customization.p is a non-readable file. I have installed the STM32CubeMx and also already tried and it works. Any ideas on how to solve these issues?
Best
Solved! Go to Solution.
2021-08-10 5:34 AM
I found that I need to go to "Configuration Parameters" and select "STM32 Options" in the Code Generation. There, I ticked "STM32CubeMx Path update". Now it works.
2021-08-10 5:34 AM
I found that I need to go to "Configuration Parameters" and select "STM32 Options" in the Code Generation. There, I ticked "STM32CubeMx Path update". Now it works.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.