2019-01-11 8:34 AM
Hi,
I am using Atollic TrueSTUDIO for STM32 and the STLINK v2 debugger found on most ST dev boards. uC is STM32L476RE if thats needed.
I am trying to get semihosting to work for printf. (SDO pin is not available in my project for ITM). I have used semihosting successfully with a different IDE before.
1) So I have changed the Properties->C/C++ Build->Settings->C Linker -> Miscellaneous->Other options to include "-specs=rdimon.specs -lc -lrdimon" (default already has nano and nospecs)
2) Have put the function declaration extern void initialise_monitor_handles(void); in main.c
3) initialise_monitor_handles() is called from main()
4) Have added "monitor arm semihosting enable" to Debug Configurations->StartupScripts->Target Hardware initialization scripts (Had it under Target Software Startup Scripts before but when debugging there was a warning message box "Failure at line:x in Target Startup Scripts: Please edit the debug configuration settings. Protocol error with Rcmd", so I assume it goes under the hardware startup scripts?
The project compiles, but when its run it breaks and Atollic opens a new tab saying "No source available for initialse_monitor_handles() at 0x8008ef4"
Any ideas? I have googled extensively.
Thanks
2019-01-14 12:25 AM
So I gave up on the semihosting and am just using uart instead. In any case, its much faster than semihosting
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.