2019-06-27 4:35 AM
I try to create a project from directory (STM32Cube_FW_L4_V1.14.0\Projects\32L476GDISCOVERY\Demonstrations\TrueSTUDIO). It creates two projects: "TrueSTUDIO" and "STM32L476G-Discovery" . The file TrueSTUDIO_converter.log is generated in the folder TrueSTUDIO. It says:
Project: TrueSTUDIO
Converter: IARProjectParser
Date: 20190627
Failed to parse IAR project format file, if possible please send the Project.ewp file together with the workspace log file to Atollic support.
When I try to build the project "STM32L476G-Discovery" an error occures:
...
In file included from ..\..\..\Core\Src\main.c:34:0:
../../../Modules/guitartuner/guitartuner.h:33:22: fatal error: arm_math.h: No such file or directory
#include "arm_math.h"
^
compilation terminated.
21:24:44 Build Finished (took 39s.82ms)
Could anybody help me?
2019-06-27 4:39 AM
Make sure you have Include paths defined in the project so it knows where to search for CMSIS include files, or if it copied them to the local project workspace.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.