2026-04-23 5:04 AM
Hello Community,
I'm trying to interface STM32 P-NUCLEO-WB55 with ADS1293 via SPI communication protocol, But there is a issue I'm unable to read data, to verify the SPI I tried to print "Reg10 = %d\r\n" but it is returning zero as value. I'm attaching the connections diagram and ioc diagram and code file, Can anyone please help me with where I'm getting wrong..
Thank you
2026-04-23 5:10 AM
Welcome @tejasharma13, to the community!
I’m afraid there won’t be much we can do to help you here. A similar question was already asked here, and it was explained to the person asking that the question would probably be better suited to TI.
Hope that helps?
Regards
/Peter
2026-04-23 5:24 AM
Hey Peter, Thanks for the reply
The reply on that question says that it would be appropriate to inquire in TI, but I have used the same breakout board with Arduino Nano and achieved results. However, when I attempted to connect it with Nucleo, the values did not appear.
2026-04-23 5:29 AM
Are you sure you can send commands like "REG0=..\r\n" directly to the chip?
I assume you have to send something like a command in one byte and some data (like reg number) in another byte and send this via SPI. Maybe on Arduino you used some lib which translates a text command to the format required by the chip?
I found a description at https://www.ti.com/lit/ds/symlink/ads1293.pdf?ts=1776946446158&ref_url=https%253A%252F%252Fwww.ti.com%252Fproduct%252Fde-de%252FADS1293
If it describes your chip I see nothing like your command "REG...=...".
2026-04-23 9:46 PM - edited 2026-04-23 9:48 PM
Hey thanks for reply,
You're right....ADS1293 does not accept commands like "REG...=..." .
It uses SPI with a binary protocol as described in the datasheet. In my implementation, I’m sending register address and data as raw bytes, I’ve written a function that formats the SPI transaction based on the datasheet.
ADS1293_ReadReg(reg) sends reg 0x80, dummy and reads back the value
This matches the SPI communication format specified in the datasheet and also I have used " https://github.com/Protocentral/protocentral-ads1293-arduino " this library for Arduino.
Can you please go through the code text file which I have attached for details....
2026-04-26 7:10 AM
How about ground? Is the GND connected between the boards?
2026-04-26 10:48 PM
Yes :)
2026-04-27 4:21 AM
Great. Get a simple logic analyzer, connect to MOSI and SCK, see if these signals go out on the wires at all. Please don't tell us that you cannot find a simple logic analyzer :)
2026-04-27 4:38 AM
So have you done as advised in that other thread:
@tejasharma13 wrote:I have used the same breakout board with Arduino Nano and achieved results. .
So use your logic analyser to capture traces of both the Arduino and Nucleo cases.
Compare and contrast ...
2026-04-27 8:00 AM
Sure, We have one in office...I'll try that
Thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.