2025-04-21 4:01 PM
I would like to know if the M95P32 EEPROM can be used by the OctoSPI interface on a STM32L4R9 processor in memory mapped mode? And if so, is there an example of a driver available?
2025-04-22 12:49 AM
Hello @erussell ;
The OctoSPI interface can be used to manage a single, dual, quad or octo SPI.
In that way, you will have the flexibility to communicate with the M95P32 in single, dual or quad SPI.
Please take a look to these posts:
- Could you kindly share any reference schematics for SPI EEPROM M95P32-I interfacing with STM32 MCU?
- Solved: M95P32 EEPROM using QSPI interface on Nucleo-L496ZGP
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-22 11:44 AM
Thank you for your response. Yes I had read those previous posts. I do understand that the M95P32 EEPROM can be connected to the OctoSPI interface on the STM32L4R9 processor but I wanted to know whether the memory mapped mode could be used. I didn't see that as specifically addressed.
2025-04-22 12:15 PM
If you can read it via standard command methods, ie a CMD +3 or +4 byte addressing, then this is used as a TEMPLATE for the Memory Mapped Mode, where the HW substitutes the masked address of the memory access into the interaction with the memory
ie 0x90000000 in STM32 memory space is 0 (zero) in the memories address space.
The mode can be 1, 2 or 4-bit, whatever you have the memory operating in, or the command used.
2025-04-24 1:08 PM
Ok - thanks. I had seen an earlier post regarding a similar question involving a STM32G4 and its quadSPI interface and the answer seemed to indicate that memory mapped mode could only be used for Reads. But I wasn't sure whether the response meant the normal SPI interface or the quadSPI interface. Anyway I will assume that I can use the memory mapped mode with the octoSPI interface.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.