2013-01-11 11:29 AM
Hi.
How i can get runtime data out of SMT32? The need is to analyze and tune filter outputs and overall process. Currently I am using SMT32 discovery board. And my development tools are Keil uVison v4.6 with ST link v2.60.Is there a way to do some kind of simple logging. To a file perhaps. Some register or variable values. From Keil IDE maybe ... ST LINK? The plan is to tune application before deployment. To emulate sensor (with dummy for loops) values and at the same time look at output behavior. Thank you in advance! #loggin-keil-smt32-st-link-stlink2013-01-11 3:56 PM
I usually push telemetry data out of a serial port. If you are logging very large amounts of data you could perhaps attach a MicroSD card, add some driver code, and a file system. You could easily record 32GB of data.
You could try the SWV feature of the debug interface, but I'm not convinced the ST-Link supports it, or that it's particularly efficient. BTW it's STM32 not SMT322013-01-12 4:01 AM
Thank you for your reply.
Thant could be a great, a optimal way to do the logging. This way could be very useful during deployment and tuning of application. But it does require some external hardware and additional software.I had something like debug.log file that is generated during Keil debugging process in in mind. A very simple way. Someting like SDOUT logging.2013-01-12 6:14 AM
There is a technique call semi-hosting
http://www.keil.com/support/man/docs/ARMCCREF/armccref_Bgbjjgij.htm
http://www.keil.com/support/man/docs/armlib/armlib_Cihibfib.htm
There is also retargeting, which redirects STDIO printf, putchar, etc out a serial port.http://www.keil.com/support/man/docs/gsac/gsac_retargetcortex.htm
I'm not sure if semi-hosting will provide the bandwidth you need, you'll need to evaluate it.2013-01-12 7:36 AM
I'm not sure if semi-hosting will provide the bandwidth you need, you'll need to evaluate it.
Usually not. At least for SWD on the discovery board, it's comparable to a 300...600 bps serial link, in other words, painfully slow. But at least it is better than nothing. For higher speeds and/or greater data volumes, a separate RS232 link served me well, too.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.